Structure represents the BLE CBFC (Credit Based Flow Control) disconnection.

This structure is used to define the parameters for a BLE CBFC disconnection, which includes the address of the remote device and the Local Channel Identifier (LCID).

Public Attributes#

uint8_t

Address of the remote device.

uint16_t

Local Channel Identifier (LCID)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_cbfc_disconn_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device.


lcid#

uint16_t rsi_ble_cbfc_disconn_s::lcid

Local Channel Identifier (LCID)