Structure represents the BLE request to read PHY.

This structure is used to define the parameter for a BLE request to read the PHY, which includes the address of the connected device.

Public Attributes#

uint8_t

Address of the connected device.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_read_phy_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device.