Structure represents the BLE request for a long attribute value.

This structure is used to define the parameters for a BLE request to get a long attribute value, which includes the remote device address, the attribute handle, and the attribute value offset.

Public Attributes#

uint8_t

Remote device address.

uint16_t

Attribute handle.

uint16_t

Attribute value offset.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_long_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address.


handle#

uint16_t rsi_ble_req_long_att_value_s::handle

Attribute handle.


offset#

uint16_t rsi_ble_req_long_att_value_s::offset

Attribute value offset.