You are viewing documentation for version:
PDFStructure represents the BLE Credit Based Flow Control (CBFC) data transmission.
This structure is used to define the parameters for a BLE CBFC data transmission, which includes the address of the remote device, the Local Channel Identifier (LCID), the length of the data to be transmitted, and the data to be transmitted.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cbfc_data_tx_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device
lcid#
uint16_t rsi_ble_cbfc_data_tx_s::lcid
Local Channel Identifier (LCID)
len#
uint16_t rsi_ble_cbfc_data_tx_s::len
Length of the data to be transmitted
data#
uint8_t rsi_ble_cbfc_data_tx_s::data[RSI_DEV_ATT_LEN]
Data to be transmitted