You are viewing documentation for version:
PDFStructure represents the BLE command to update connection parameters.
This structure is used to define the parameters for a BLE command to update connection parameters, which includes the address of the connected device, minimum and maximum connection intervals, peripheral latency, and supervision timeout.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cmd_conn_params_update_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device
min_interval#
uint16_t rsi_ble_cmd_conn_params_update_s::min_interval
Minimum connection interval
max_interval#
uint16_t rsi_ble_cmd_conn_params_update_s::max_interval
Maximum connection interval
latency#
uint16_t rsi_ble_cmd_conn_params_update_s::latency
Peripheral latency
timeout#
uint16_t rsi_ble_cmd_conn_params_update_s::timeout
Supervision timeout