You are viewing documentation for version:
PDFStructure representing the BLE start encryption request.
This structure is used to define the parameters for a BLE start encryption request, which includes the address of the connected device, the remote device's Encrypted Diversifier (EDIV) value, Random (RAND) value, and Long Term Key (LTK) value.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_start_encryption_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device
ediv#
uint16_t rsi_ble_start_encryption_s::ediv
Remote device EDIV value
rand#
uint8_t rsi_ble_start_encryption_s::rand[8]
Remote device RAND value
ltk#
uint8_t rsi_ble_start_encryption_s::ltk[16]
Remote device LTK value