You are viewing documentation for version:
PDFStructure represents the BLE request to enable or disable address resolution.
This structure is used to define the parameters for a BLE request to enable or disable address resolution, which includes the enable flag, reserved field for future use, and the timeout value for address resolution.
Public Attribute Documentation#
enable#
uint8_t rsi_ble_set_addr_resolution_enable_s::enable
Enable or disable address resolution
reserved#
uint8_t rsi_ble_set_addr_resolution_enable_s::reserved
Reserved for future use
tout#
uint16_t rsi_ble_set_addr_resolution_enable_s::tout
Timeout value for address resolution