You are viewing documentation for version:
PDFStructure represents the BLE request for multiple attribute values.
This structure is used to define the parameters for a BLE request to get multiple attribute values, which includes the remote device address, the number of attribute handles, reserved bytes for future use, and the list of attribute handles.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_multiple_att_val_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
num_of_handles#
uint8_t rsi_ble_req_multiple_att_val_s::num_of_handles
Number of attribute handles
reserved#
uint8_t rsi_ble_req_multiple_att_val_s::reserved
Reserved for future use
handles#
uint16_t rsi_ble_req_multiple_att_val_s::handles[RSI_BLE_MAX_RESP_LIST]
List of attribute handles