You are viewing documentation for version:
PDFStructure represents the BLE Security Manager Protocol (SMP) pairing request.
This structure is used to define the parameters for a BLE SMP pairing request, which includes the device address, IO capability, and MITM (Man-In-The-Middle) protection requirement.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_smp_pair_s::dev_addr[RSI_DEV_ADDR_LEN]
Device address for the pairing request
io_capability#
uint8_t rsi_ble_req_smp_pair_s::io_capability
IO capability of the device
mitm_req#
uint8_t rsi_ble_req_smp_pair_s::mitm_req
MITM (Man-In-The-Middle) protection requirement