You are viewing documentation for version:
PDFStructure represents the BLE notification for an attribute value.
This structure is used to define the parameters for a BLE notification of an attribute value, which includes the remote device address, the attribute handle, the length of the attribute value, and the attribute value itself.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_notify_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
handle#
uint16_t rsi_ble_notify_att_value_s::handle
Attribute handle
data_len#
uint16_t rsi_ble_notify_att_value_s::data_len
Attribute value length
data#
uint8_t rsi_ble_notify_att_value_s::data[RSI_DEV_ATT_LEN]
Attribute value (data)