You are viewing documentation for version:
PDFStructure represents the BLE request to set PHY.
This structure is used to define the parameters for a BLE request to set the PHY, which includes the address of the connected device, all PHYs preference, preferred TX PHY, preferred RX PHY, reserved field for future use, and PHY options.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_phy_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device
all_phy#
uint8_t rsi_ble_set_phy_s::all_phy
All PHYs preference
tx_phy#
uint8_t rsi_ble_set_phy_s::tx_phy
Preferred TX PHY
rx_phy#
uint8_t rsi_ble_set_phy_s::rx_phy
Preferred RX PHY
reserved#
uint8_t rsi_ble_set_phy_s::reserved
Reserved for future use
phy_options#
uint16_t rsi_ble_set_phy_s::phy_options
PHY options