You are viewing documentation for version:
PDFStructure represents the Bluetooth response to get the local device name.
This structure is used to define the parameters for the response that includes the local Bluetooth device name, that includes the name length, the name itself, and a reserved variable.
Public Attribute Documentation#
name_len#
uint8_t rsi_bt_resp_get_local_name_s::name_len
Name length
name#
int8_t rsi_bt_resp_get_local_name_s::name[RSI_DEV_NAME_LEN]
Array which consists name of the local device. The maximum size of this array is 50
_reserved#
uint8_t rsi_bt_resp_get_local_name_s::_reserved
Reserved variable