Plugin Commands: IAS Zone Server
Macros | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_STATUS |
plugin ias-zone-server changeStatus [newStatus:2] [timeSinceOccurredSeconds:1] [endpoint:1] | |
#define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_INFO |
plugin ias-zone-server info [endpoint:1] |
Detailed Description
This plugin provides a set of CLI commands for managing the local IAS Zone server.
Macro Definition Documentation
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_CHANGE_STATUS |
plugin ias-zone-server changeStatus [newStatus:2] [timeSinceOccurredSeconds:1] [endpoint:1]
- Update the zone status attribute of a given endpoint's IAS Zone cluster to the given value
- newStatus - INT16U - The new status to be written
- timeSinceOccurredSeconds - INT8U - The amount time that has passed since the last update occurred (seconds)
- endpoint - INT8U - The endpoint whose zone status attribute is to be updated
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_IAS_ZONE_SERVER_PLUGIN_IAS_ZONE_SERVER_INFO |
plugin ias-zone-server info [endpoint:1]
- Print current value of the following cluster attributes: zone type, zone state, zone status, zone id
- endpoint - INT8U - The endpoint whose IAS Zone Cluster information is to be printed