Zigbee Internet Client/Server Remote Binding struct.

#include < af-types.h >

Data Fields

EmberEUI64 targetEUI64
uint8_t sourceEndpoint
uint8_t destEndpoint
uint16_t clusterId
EmberEUI64 destEUI64
EmberEUI64 sourceEUI64

Zigbee Internet Client/Server Remote Binding struct.

Field Documentation

uint16_t EmberAfRemoteBindingStruct::clusterId
uint8_t EmberAfRemoteBindingStruct::destEndpoint
EmberEUI64 EmberAfRemoteBindingStruct::destEUI64
uint8_t EmberAfRemoteBindingStruct::sourceEndpoint
EmberEUI64 EmberAfRemoteBindingStruct::sourceEUI64
EmberEUI64 EmberAfRemoteBindingStruct::targetEUI64

The documentation for this struct was generated from the following file:
  • af-types.h