End Devices
EmberZNet API relating to end device children.
Functions |
|
| EmberNodeId | emberChildId (uint8_t childIndex) |
|
Converts a child index to a node ID.
|
|
| int8_t | emberChildPower (uint8_t childIndex) |
|
This function returns radio power value of the child from the given childIndex.
|
|
| void | emberSetChildPower (uint8_t childIndex, int8_t newPower) |
|
This function sets the radio power value for a given child index.
|
|
| uint8_t | emberChildIndex ( EmberNodeId childId) |
|
Converts a node ID to a child index.
|
|
| EmberStatus | emberGetChildData (uint8_t index, EmberChildData *childData) |
|
Gets the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns
EMBER_NOT_JOINED
. Possible child indexes run from zero to
emberMaxChildCount()
- 1.
|
|
| void | emberChildJoinHandler (uint8_t index, bool joining) |
|
Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.
|
|
| EmberStatus | emberPollForData (void) |
|
Requests any pending data from the parent node. This function allows an end device to query its parent for any pending data.
|
|
| void | emberSetMacPollCcaWaitTime (uint8_t waitBeforeRetryIntervalMs) |
| void | emberPollCompleteHandler ( EmberStatus status) |
| EmberStatus | emberSetMessageFlag ( EmberNodeId childId) |
|
Sets a flag to indicate that there is a message pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from emberPollHandler, which is called when the child requests data.
|
|
| EmberStatus | emberClearMessageFlag ( EmberNodeId childId) |
|
Clears a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.
|
|
| void | emberPollHandler ( EmberNodeId childId, bool transmitExpected) |
|
Called to allow the application to send a message in response to a poll from a child.
|
|
| uint8_t | emberChildCount (void) |
|
Returns the number of children the node currently has.
|
|
| uint8_t | emberRouterChildCount (void) |
|
Returns the number of router children that the node currently has.
|
|
| uint8_t | emberMaxChildCount (void) |
|
Returns the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.
|
|
| uint8_t | emberMaxRouterChildCount (void) |
|
Returns the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.
|
|
| EmberNodeId | emberGetParentNodeId (void) |
|
Returns the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).
|
|
| EmberEUI64 | emberGetParentEui64 (void) |
|
Returns the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).
|
|
Power Management |
|
| enum |
{
EMBER_OUTGOING_MESSAGES = 0x0001, EMBER_INCOMING_MESSAGES = 0x0002, EMBER_RADIO_IS_ON = 0x0004, EMBER_TRANSPORT_ACTIVE = 0x0008, EMBER_APS_LAYER_ACTIVE = 0x0010, EMBER_ASSOCIATING = 0x0020, EMBER_ZLL_TOUCH_LINKING = 0x0040, EMBER_NETWORK_TIMEOUT_REQUEST = 0x0200, EMBER_SEND_ORPHAN_NOTIFICATION = 0x0400 } |
|
Defines tasks that prevent the stack from sleeping.
|
|
| uint16_t | emberCurrentStackTasks (void) |
|
Returns a bitmask indicating the stack's current tasks.
|
|
| bool | emberOkToNap (void) |
|
Indicates whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.
|
|
| bool | emberParentTokenSet (void) |
|
Indicates whether the parent token has been set by association.
|
|
| bool | emberOkToHibernate (void) |
|
Indicates whether the stack currently has any tasks pending.
|
|
| bool | emberOkToGoToLowPowerMode (void) |
|
Indicates whether the stack is ready to go into low power (EM4) mode.
|
|
| bool | emberOkToLongPoll (void) |
|
Indicates whether the stack is currently in a state that does not require the application to periodically poll.
|
|
| void | emberStackPowerDown (void) |
|
Immediately turns the radio power completely off.
|
|
| void | emberStackPowerUp (void) |
|
Initializes the radio. Typically called coming out of deep sleep.
|
|
| #define | EMBER_HIGH_PRIORITY_TASKS ( EMBER_OUTGOING_MESSAGES | EMBER_INCOMING_MESSAGES | EMBER_RADIO_IS_ON ) |
|
A mask of the tasks that prevent a device from sleeping.
|
|
Detailed Description
EmberZNet API relating to end device children.
See
child.h
for source code.
Macro Definition Documentation
| #define EMBER_HIGH_PRIORITY_TASKS ( EMBER_OUTGOING_MESSAGES | EMBER_INCOMING_MESSAGES | EMBER_RADIO_IS_ON ) |
A mask of the tasks that prevent a device from sleeping.
Enumeration Type Documentation
| anonymous enum |
Defines tasks that prevent the stack from sleeping.
| Enumerator | |
|---|---|
| EMBER_OUTGOING_MESSAGES |
There are messages waiting for transmission. |
| EMBER_INCOMING_MESSAGES |
One or more incoming messages being processed. |
| EMBER_RADIO_IS_ON |
The radio is currently powered on. On sleepy devices, the radio is turned off when not in use. On non-sleepy devices ( EMBER_COORDINATOR , EMBER_ROUTER , or EMBER_END_DEVICE ), the radio is always on. |
| EMBER_TRANSPORT_ACTIVE |
The transport layer has messages awaiting an ACK. |
| EMBER_APS_LAYER_ACTIVE |
The ZigBee APS layer has messages awaiting an ACK. |
| EMBER_ASSOCIATING |
The node is currently trying to associate with a ZigBee PRO network. |
| EMBER_ZLL_TOUCH_LINKING |
The node is currently touch linking. |
| EMBER_NETWORK_TIMEOUT_REQUEST |
Network Timeout Request Event. |
| EMBER_SEND_ORPHAN_NOTIFICATION |
Sending Orphan Notification Event. |
Function Documentation
| uint8_t emberChildCount | ( | void |
|
) |
Returns the number of children the node currently has.
- Returns
- The number of children.
| EmberNodeId emberChildId | ( | uint8_t |
childIndex
|
) |
Converts a child index to a node ID.
- Parameters
-
childIndexThe index.
- Returns
- The node ID of the child or EMBER_NULL_NODE_ID if there isn't a child at the childIndex specified.
| uint8_t emberChildIndex | ( | EmberNodeId |
childId
|
) |
Converts a node ID to a child index.
- Parameters
-
childIdThe node ID of the child.
- Returns
- The child index or 0xFF if the node ID does not belong to a child.
| void emberChildJoinHandler | ( | uint8_t |
index,
|
| bool |
joining
|
||
| ) |
Called by the stack when a child joins or leaves. 'Joining' is true if the child is joining and false if leaving.
The index is the same as the value that should be passed to emberGetChildData() to get this child's data. Note that if the child is leaving, emberGetChildData() will return EMBER_NOT_JOINED if called with this index. If the application includes emberChildJoinHandler() , it must define EMBER_APPLICATION_HAS_CHILD_JOIN_HANDLER in its CONFIGURATION_HEADER
- Parameters
-
indexThe index of the child of interest. joiningTrue if the child is joining, false if the child is leaving.
| int8_t emberChildPower | ( | uint8_t |
childIndex
|
) |
This function returns radio power value of the child from the given childIndex.
- Parameters
-
childIndexThe index.
- Returns
- The power of the child or maximum radio power, which is the power value provided by the user while forming/joining a network if there isn't a child at the childIndex specified.
| EmberStatus emberClearMessageFlag | ( | EmberNodeId |
childId
|
) |
Clears a flag to indicate that there are no more messages for a child. The next time the child polls, it will be informed that it does not have any pending messages.
- Parameters
-
childIdThe ID of the child that no longer has pending messages.
- Returns
-
An
EmberStatusvalue.- EMBER_SUCCESS - The next time that the child polls, it will be informed that it does not have any pending messages.
- EMBER_NOT_JOINED - The child identified by childId is not our child.
| uint16_t emberCurrentStackTasks | ( | void |
|
) |
Returns a bitmask indicating the stack's current tasks.
The mask EMBER_HIGH_PRIORITY_TASKS defines which tasks are high priority. Devices should not sleep if any high priority tasks are active. Active tasks that are not high priority are waiting for messages to arrive from other devices. If there are active tasks, but no high priority ones, the device may sleep but should periodically wake up and call emberPollForData() in order to receive messages. Parents will hold messages for EMBER_INDIRECT_TRANSMISSION_TIMEOUT milliseconds before discarding them.
- Returns
- A bitmask of the stack's active tasks.
| EmberStatus emberGetChildData | ( | uint8_t |
index,
|
| EmberChildData * |
childData
|
||
| ) |
Gets the EUI64 and node type of the child at the provided index. If there is no child at 'index', it returns EMBER_NOT_JOINED . Possible child indexes run from zero to emberMaxChildCount() - 1.
- Parameters
-
indexThe index of the child of interest. childDataThe child's data is copied here.
- Returns
- Returns EMBER_SUCCESS if a child is found at that index, EMBER_NOT_JOINED if not.
| EmberEUI64 emberGetParentEui64 | ( | void |
|
) |
Returns the parent's EUI64. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).
- Returns
- The parent's EUI64.
| EmberNodeId emberGetParentNodeId | ( | void |
|
) |
Returns the parent's node ID. The return value is undefined for nodes without parents (coordinators and nodes that are not joined to a network).
- Returns
- The parent's node ID.
| uint8_t emberMaxChildCount | ( | void |
|
) |
Returns the maximum number of children for this node. The return value is undefined for nodes that are not joined to a network.
- Returns
- The maximum number of children.
| uint8_t emberMaxRouterChildCount | ( | void |
|
) |
Returns the maximum number of router children for this node. The return value is undefined for nodes that are not joined to a network.
- Returns
- The maximum number of router children.
| bool emberOkToGoToLowPowerMode | ( | void |
|
) |
Indicates whether the stack is ready to go into low power (EM4) mode.
This API is only applicable on EFR32 devices.
- Returns
- True if okay to go into energy mode four.
| bool emberOkToHibernate | ( | void |
|
) |
Indicates whether the stack currently has any tasks pending.
If there are no pending tasks, emberTick() does not need to be called until the next time a stack API function is called. This function can only be called when the node type is EMBER_SLEEPY_END_DEVICE or
- Returns
- True if the application may sleep for as long as it wishes.
| bool emberOkToLongPoll | ( | void |
|
) |
Indicates whether the stack is currently in a state that does not require the application to periodically poll.
- Returns
- True if the application may stop polling periodically.
| bool emberOkToNap | ( | void |
|
) |
Indicates whether the stack is currently in a state where there are no high-priority tasks, allowing the device to sleep.
There may be tasks expecting incoming messages, in which case the device should periodically wake up and call emberPollForData() in order to receive messages. This function can only be called when the node type is EMBER_SLEEPY_END_DEVICE
- Returns
- True if the application may sleep but the stack may be expecting incoming messages.
| bool emberParentTokenSet | ( | void |
|
) |
Indicates whether the parent token has been set by association.
- Returns
- True if the parent token has been set.
| void emberPollCompleteHandler | ( | EmberStatus |
status
|
) |
@ brief This is called by the stack when a data poll to the parent is complete.
If the application includes emberPollCompleteHandler() , it must define EMBER_APPLICATION_HAS_POLL_COMPLETE_HANDLER within its CONFIGURATION_HEADER
- Parameters
-
statusAn EmberStatusvalue:- EMBER_SUCCESS - Data was received in response to the poll.
- EMBER_MAC_NO_DATA - No data was pending.
- EMBER_DELIVERY_FAILED - The poll message could not be sent.
- EMBER_MAC_NO_ACK_RECEIVED - The poll message was sent but not acknowledged by the parent.
| EmberStatus emberPollForData | ( | void |
|
) |
Requests any pending data from the parent node. This function allows an end device to query its parent for any pending data.
End devices must call this function periodically to maintain contact with their parent. The parent will remove a child if it has not received a poll from it within the last EMBER_END_DEVICE_POLL_TIMEOUT << EMBER_END_DEVICE_POLL_TIMEOUT_SHIFT seconds.
If the end device has lost contact with its parent, emberPollForData() calls ::emberRejoinNetwork(true) and returns EMBER_ERR_FATAL .
The default values for the timeouts are set in
config/ember-configuration-defaults.h
and can be overridden in the application's configuration header.
- Returns
-
An EmberStatus value:
- EMBER_SUCCESS - The poll message has been submitted for transmission.
- EMBER_INVALID_CALL - The node is not an end device.
- EMBER_NOT_JOINED - The node is not part of a network.
- EMBER_MAC_TRANSMIT_QUEUE_FULL - The MAC layer transmit queue is full.
- EMBER_NO_BUFFERS - No buffers available to create the data poll message.
- EMBER_ERR_FATAL - Too much time has elapsed since the last successful poll. A rejoin attempt has been initiated. This error is not "fatal". The command can be retried until successful.
| void emberPollHandler | ( | EmberNodeId |
childId,
|
| bool |
transmitExpected
|
||
| ) |
Called to allow the application to send a message in response to a poll from a child.
This function is called when a child polls, provided that the pending message flag is set for that child (see emberSetMessageFlag() . The message should be sent to the child using emberSendUnicast() with the EMBER_APS_OPTION_POLL_RESPONSE option.
If the application includes ::emberPollHanlder(), it must define EMBER_APPLICATION_HAS_POLL_HANDLER in its CONFIGURATION_HEADER.
- Parameters
-
childIdThe ID of the child that is requesting data. transmitExpectedTrue if the child is expecting an application- supplied data message. False otherwise.
| uint8_t emberRouterChildCount | ( | void |
|
) |
Returns the number of router children that the node currently has.
- Returns
- The number of router children.
| void emberSetChildPower | ( | uint8_t |
childIndex,
|
| int8_t |
newPower
|
||
| ) |
This function sets the radio power value for a given child index.
- Parameters
-
childIndexThe index. newPowerThe new power value.
| void emberSetMacPollCcaWaitTime | ( | uint8_t |
waitBeforeRetryIntervalMs
|
) |
@ brief This function is useful to sleepy end devices. This function will set the retry interval (in milliseconds) for mac data poll. This interval is the time in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason.
- Parameters
-
waitBeforeRetryIntervalMsTime in milliseconds the device waits before retrying a data poll when a MAC level data poll fails for any reason
| EmberStatus emberSetMessageFlag | ( | EmberNodeId |
childId
|
) |
Sets a flag to indicate that there is a message pending for a child. The next time that the child polls, it will be informed that it has a pending message. The message is sent from emberPollHandler, which is called when the child requests data.
- Parameters
-
childIdThe ID of the child that just polled for data.
- Returns
-
An
EmberStatusvalue.- EMBER_SUCCESS - The next time that the child polls, it will be informed that it has pending data.
- EMBER_NOT_JOINED - The child identified by childId is not our child.
| void emberStackPowerDown | ( | void |
|
) |
Immediately turns the radio power completely off.
Calling this function will render all other stack functions except emberStackPowerUp() non-functional until the radio is powered back on.
| void emberStackPowerUp | ( | void |
|
) |
Initializes the radio. Typically called coming out of deep sleep.
For non-sleepy devices, also turns the radio on and leaves it in RX mode.