EmberTransientKeyData Struct Reference
This data structure contains the transient key data that is used during Zigbee 3.0 joining.
#include <
ember-types.h
>
Data Fields |
|
| EmberEUI64 | eui64 |
| EmberKeyData | keyData |
| uint32_t | incomingFrameCounter |
| uint32_t | countdownTimerMs |
| EmberKeyStructBitmask | bitmask |
This data structure contains the transient key data that is used during Zigbee 3.0 joining.
Field Documentation
| EmberKeyStructBitmask EmberTransientKeyData::bitmask |
| uint32_t EmberTransientKeyData::countdownTimerMs |
| EmberEUI64 EmberTransientKeyData::eui64 |
| uint32_t EmberTransientKeyData::incomingFrameCounter |
| EmberKeyData EmberTransientKeyData::keyData |
The documentation for this struct was generated from the following file:
-
ember-types.h