InterPanHeader Struct Reference
A struct for keeping track of all of the header info.
#include <
ami-inter-pan.h
>
Data Fields |
|
| uint8_t | messageType |
| uint16_t | panId |
| bool | hasLongAddress |
| EmberNodeId | shortAddress |
| EmberEUI64 | longAddress |
| uint16_t | profileId |
| uint16_t | clusterId |
| uint16_t | groupId |
A struct for keeping track of all of the header info.
A struct for keeping track of all of the interpan header info.
Field Documentation
| uint16_t InterPanHeader::clusterId |
| uint16_t InterPanHeader::groupId |
| bool InterPanHeader::hasLongAddress |
| EmberEUI64 InterPanHeader::longAddress |
| uint8_t InterPanHeader::messageType |
| uint16_t InterPanHeader::panId |
| uint16_t InterPanHeader::profileId |
| EmberNodeId InterPanHeader::shortAddress |
The documentation for this struct was generated from the following files:
-
ami-inter-pan.h -
ami-inter-pan-host.h