Information about the ZLL network and specific device that responded to a ZLL scan request.

#include < zll-types.h >

Data Fields

EmberZigbeeNetwork zigbeeNetwork
EmberZllSecurityAlgorithmData securityAlgorithm
EmberEUI64 eui64
EmberNodeId nodeId
EmberZllState state
EmberNodeType nodeType
uint8_t numberSubDevices
uint8_t totalGroupIdentifiers
uint8_t rssiCorrection

Information about the ZLL network and specific device that responded to a ZLL scan request.

Field Documentation

EmberEUI64 EmberZllNetwork::eui64
EmberNodeId EmberZllNetwork::nodeId
EmberNodeType EmberZllNetwork::nodeType
uint8_t EmberZllNetwork::numberSubDevices
uint8_t EmberZllNetwork::rssiCorrection
EmberZllSecurityAlgorithmData EmberZllNetwork::securityAlgorithm
EmberZllState EmberZllNetwork::state
uint8_t EmberZllNetwork::totalGroupIdentifiers
EmberZigbeeNetwork EmberZllNetwork::zigbeeNetwork

The documentation for this struct was generated from the following file:
  • zll-types.h