Describes the Initial Security features and requirements that will be used when forming or joining ZigBee Light Link networks.

#include < zll-types.h >

Data Fields

uint32_t bitmask
EmberZllKeyIndex keyIndex
EmberKeyData encryptionKey
EmberKeyData preconfiguredKey

Describes the Initial Security features and requirements that will be used when forming or joining ZigBee Light Link networks.

Field Documentation

uint32_t EmberZllInitialSecurityState::bitmask

This bitmask is unused. All values are reserved for future use.

EmberKeyData EmberZllInitialSecurityState::encryptionKey

The encryption key for use by algorithms that require it.

EmberZllKeyIndex EmberZllInitialSecurityState::keyIndex

The key encryption algorithm advertised by the application.

EmberKeyData EmberZllInitialSecurityState::preconfiguredKey

The pre-configured link key used during classical ZigBee commissioning.


The documentation for this struct was generated from the following file:
  • zll-types.h