Stack Information
Data Structures |
|
| struct | EmberEndpointDescription |
|
Endpoint information (a ZigBee Simple Descriptor).
|
|
| struct | EmberEndpoint |
|
Gives the endpoint information for a particular endpoint.
|
|
Macros |
|
| #define | EMBER_MAJOR_VERSION 6 |
| #define | EMBER_MINOR_VERSION 4 |
| #define | EMBER_PATCH_VERSION 0 |
| #define | EMBER_SPECIAL_VERSION 0 |
| #define | EMBER_BUILD_NUMBER 385 |
| #define | EMBER_FULL_VERSION |
| #define | EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA |
| #define | SOFTWARE_VERSION EMBER_FULL_VERSION |
Functions |
|
| void | emberStackStatusHandler ( EmberStatus status) |
|
A callback invoked when the status of the stack changes. If the status parameter equals
EMBER_NETWORK_UP
, the
emberGetNetworkParameters()
function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
|
|
| EmberNetworkStatus | emberNetworkState (void) |
|
Returns the current join status.
|
|
| bool | emberStackIsUp (void) |
|
Indicates whether the stack is currently up.
|
|
| EmberStatus | emberWriteNodeData (bool erase) |
|
Writes node data to stack token.
|
|
| EmberEUI64 | emberGetEui64 (void) |
|
Returns the EUI64 ID of the local node.
|
|
| bool | emberIsLocalEui64 ( EmberEUI64 eui64) |
Determines whether
eui64
is the local node's EUI64 ID.
|
|
| EmberNodeId | emberGetNodeId (void) |
|
Returns the 16-bit node ID of local node on the current logical network.
|
|
| EmberNodeId | emberRadioGetNodeId (void) |
|
Returns the 16-bit node ID of local node on the network it is currently tuned on.
|
|
| void | emberSetManufacturerCode (uint16_t code) |
|
Sets the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
|
|
| void | emberSetPowerDescriptor (uint16_t descriptor) |
|
Sets the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
|
|
| void | emberSetMaximumIncomingTransferSize (uint16_t size) |
|
Sets the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
|
|
| void | emberSetMaximumOutgoingTransferSize (uint16_t size) |
|
Sets the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
|
|
| void | emberSetDescriptorCapability (uint8_t capability) |
|
Sets the descriptor capability field of the node.
|
|
| EmberStatus | emberGetNetworkParameters ( EmberNetworkParameters *parameters) |
|
Copies the current network parameters into the structure provided by the caller.
|
|
| EmberStatus | emberGetRadioParameters (uint8_t phyIndex, EmberMultiPhyRadioParameters *parameters) |
|
Copies the current radio parameters into the structure provided by the caller.
|
|
| EmberStatus | emberGetNodeType ( EmberNodeType *resultLocation) |
|
Copies the current node type into the location provided by the caller.
|
|
| EmberStatus | emberSetRadioChannel (uint8_t channel) |
|
Sets the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
|
|
| uint8_t | emberGetRadioChannel (void) |
|
Gets the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
|
|
| EmberStatus | emberSetRadioPower (int8_t power) |
|
Sets the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
|
|
| int8_t | emberGetRadioPower (void) |
|
Gets the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
|
|
| EmberPanId | emberGetPanId (void) |
|
Returns the local node's PAN ID of the current logical network.
|
|
| EmberPanId | emberRadioGetPanId (void) |
|
Returns the local node's PAN ID of the current radio network.
|
|
| void | emberGetExtendedPanId (uint8_t *resultLocation) |
|
Fetches a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see
emberNetworkState
), the Extended PAN ID returned will be an invalid value.
|
|
| uint8_t | emberGetEndpoint (uint8_t index) |
Retrieves the endpoint number for the index'th endpoint.
index
must be less than the value of emberEndpointCount.
|
|
| bool | emberGetEndpointDescription (uint8_t endpoint, EmberEndpointDescription *result) |
|
Retrieves the endpoint description for the given endpoint.
|
|
| uint16_t | emberGetEndpointCluster (uint8_t endpoint, EmberClusterListId listId, uint8_t listIndex) |
|
Retrieves a cluster ID from one of the cluster lists associated with the given endpoint.
|
|
| bool | emberIsNodeIdValid ( EmberNodeId nodeId) |
Determines whether
nodeId
is valid.
|
|
| EmberNodeId | emberLookupNodeIdByEui64 ( EmberEUI64 eui64) |
|
Returns the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
|
|
| EmberStatus | emberLookupEui64ByNodeId ( EmberNodeId nodeId, EmberEUI64 eui64Return) |
|
Returns the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
|
|
| void | emberCounterHandler ( EmberCounterType type, EmberCounterInfo info) |
|
A callback invoked to inform the application of the occurrence of an event defined by
EmberCounterType
, for example, transmissions and receptions at different layers of the stack.
|
|
| bool | emberCounterRequiresPhyIndex ( EmberCounterType type) |
| bool | emberCounterRequiresDestinationNodeId ( EmberCounterType type) |
| void | emberStackTokenChangedHandler (uint16_t tokenAddress) |
|
A callback invoked to inform the application that a stack token has changed.
|
|
| bool | emberRtosIdleHandler (uint32_t *idleTimeMs) |
|
A callback to allow the application to manage idling the MCU.
|
|
| void | emberRtosStackWakeupIsrHandler (void) |
|
A callback to request the application to wake up the stack task.
|
|
| EmberStatus | emberGetNeighbor (uint8_t index, EmberNeighborTableEntry *result) |
Copies a neighbor table entry to the structure that
result
points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using
emberNeighborCount()
.
|
|
| EmberStatus | emberSetRoutingShortcutThreshold (uint8_t costThresh) |
|
Sets the routing shortcut threshold to directly use a neighbor instead of performing routing.
|
|
| uint8_t | emberGetRoutingShortcutThreshold (void) |
|
Gets the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
|
|
| EmberStatus | emberSetInitialNeighborOutgoingCost (uint8_t cost) |
|
Sets neighbor's initial outgoing link cost.
|
|
| uint8_t | emberGetInitialNeighborOutgoingCost (void) |
|
Gets neighbor's initial outgoing link cost.
|
|
| void | emberResetRejoiningNeighborsFC (bool reset) |
|
Indicates whether a rejoining neighbor's incoming FC should be reset.
|
|
| bool | emberIsResetRejoiningNeighborsFCEnabled (void) |
|
Checks if resetting the incoming FC for a rejoining neighbor is enabled.
|
|
| EmberStatus | emberGetRouteTableEntry (uint8_t index, EmberRouteTableEntry *result) |
Copies a route table entry to the structure that the
result
points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via
emberRouteTableSize()
.
|
|
| uint8_t | emberStackProfile (void) |
|
Returns the stack profile of the network which the node has joined.
|
|
| uint8_t | emberTreeDepth (void) |
|
Returns the depth of the node in the network.
|
|
| uint8_t | emberNeighborCount (void) |
|
Returns the number of active entries in the neighbor table.
|
|
| uint8_t | emberRouteTableSize (void) |
|
Returns the size of the route table.
|
|
| uint8_t | emberNextZigbeeSequenceNumber (void) |
|
Increments and returns the Zigbee sequence number.
|
|
| uint8_t | emberGetMaxNwkRetries (void) |
|
Get max number of NWK retries.
|
|
| EmberStatus | emberGetBeaconClassificationParams ( EmberBeaconClassificationParams *param) |
|
API used to get current beacon classification parameter settings.
|
|
| EmberStatus | emberSetBeaconClassificationParams ( EmberBeaconClassificationParams *param) |
|
API used to set current beacon classification parameters.
|
|
Variables |
|
| PGM uint8_t | emberStackProfileId [] |
|
The application must provide a definition for this variable.
|
|
| uint8_t | emberEndpointCount |
|
The application must provide a definition for this variable.
|
|
| EmberEndpoint | emberEndpoints [] |
|
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
|
|
Radio-specific Functions |
|
| EmberStatus | emberSetTxPowerMode (uint16_t txPowerMode) |
|
Enables boost power mode and/or the alternate transmit path.
|
|
| uint16_t | emberGetTxPowerMode (void) |
|
Returns the current configuration of boost power mode and alternate transmitter output.
|
|
| EmberStatus | emberSetNodeId ( EmberNodeId nodeId) |
|
Sets the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
|
|
| uint8_t | emberGetPhyInterfaceCount (void) |
|
Returns the number of PHY interfaces present.
|
|
| void | emberRadioNeedsCalibratingHandler (void) |
|
The radio calibration callback function.
|
|
| void | emberCalibrateCurrentChannel (void) |
|
Calibrates the current channel. The stack will notify the application of the need for channel calibration via the
emberRadioNeedsCalibratingHandler()
callback function during
emberTick()
. This function should only be called from within the context of the
emberRadioNeedsCalibratingHandler()
callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
|
|
| void | emberSetLongUpTime (bool hasLongUpTime) |
|
sets the device uptime to be long or short the uptime is then advertised in the beacons
|
|
| void | emberSetHubConnectivity (bool connected) |
|
sets the hub connectivity to be true or false the hub connectivity is then advertised in the beacons
|
|
| bool | emberIsUpTimeLong (void) |
| bool | emberIsHubConnected (void) |
| EmberStatus | emberRadioGetSchedulerPriorities ( EmberMultiprotocolPriorities *priorities) |
|
API used to get current zigbee priorities being used in multiprotocol applications. See UG305, the Dynamic Multiprotocol User Guide for more info on recommended priorities and discussion regarding interactivity with other stacks.
|
|
Detailed Description
See
stack-info.h
for source code.
See also
config.h
.
This documentation was produced from the following software release and build.
| SOFTWARE_VERSION | 0x4700 | High byte = release number, low byte = patch number |
Macro Definition Documentation
| #define EMBER_BUILD_NUMBER 385 |
| #define EMBER_FULL_VERSION |
| #define EMBER_MAJOR_VERSION 6 |
| #define EMBER_MINOR_VERSION 4 |
| #define EMBER_PATCH_VERSION 0 |
| #define EMBER_SPECIAL_VERSION 0 |
| #define EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA |
| #define SOFTWARE_VERSION EMBER_FULL_VERSION |
Software version. High byte = release number, low byte = patch number.
Function Documentation
| void emberCalibrateCurrentChannel | ( | void |
|
) |
Calibrates the current channel. The stack will notify the application of the need for channel calibration via the emberRadioNeedsCalibratingHandler() callback function during emberTick() . This function should only be called from within the context of the emberRadioNeedsCalibratingHandler() callback function. Calibration can take up to 150 ms. Note if this function is called when the radio is off, it will turn the radio on and leave it on.
| void emberCounterHandler | ( | EmberCounterType |
type,
|
| EmberCounterInfo |
info
|
||
| ) |
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType , for example, transmissions and receptions at different layers of the stack.
The application must define ::EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
- Parameters
-
typeType of the event. infocould map to: - data: For transmission events, the number of retries used. For most other events, this parameter is unused and is set to zero.
- phyIndex: use for mac specific counters specifying if they belong to sub-Ghz or 2.4 GHz.
- destinationNodeId: identifying which connection/destinationId a specific counter refers to.
- Any combination of the parameters above.
| bool emberCounterRequiresDestinationNodeId | ( | EmberCounterType |
type
|
) |
| bool emberCounterRequiresPhyIndex | ( | EmberCounterType |
type
|
) |
| EmberStatus emberGetBeaconClassificationParams | ( | EmberBeaconClassificationParams * |
param
|
) |
API used to get current beacon classification parameter settings.
| uint8_t emberGetEndpoint | ( | uint8_t |
index
|
) |
Retrieves the endpoint number for the index'th endpoint.
index
must be less than the value of emberEndpointCount.
This function is provided by the stack, using the data from emberEndpoints, unless the application defines EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
- Parameters
-
indexThe index of an endpoint (as distinct from its endpoint number). This must be less than the value of emberEndpointCount.
- Returns
- The endpoint number for the index'th endpoint.
| uint16_t emberGetEndpointCluster | ( | uint8_t |
endpoint,
|
| EmberClusterListId |
listId,
|
||
| uint8_t |
listIndex
|
||
| ) |
Retrieves a cluster ID from one of the cluster lists associated with the given endpoint.
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
- Parameters
-
endpointThe endpoint from which the cluster ID is to be read. listIdThe list from which the cluster ID is to be read. listIndexThe index of the desired cluster ID in the list. This value must be less than the length of the list. The length can be found in the EmberEndpointDescription for this endpoint.
- Returns
- The cluster ID at position listIndex in the specified endpoint cluster list.
| bool emberGetEndpointDescription | ( | uint8_t |
endpoint,
|
| EmberEndpointDescription * |
result
|
||
| ) |
Retrieves the endpoint description for the given endpoint.
This function is provided by the stack, using the data from emberEndpoints, unless the application defines ::EMBER_APPLICATION_HAS_GET_ENDPOINT in its ::CONFIGURATION_HEADER.
- Parameters
-
endpointThe endpoint whose description is to be returned. resultA pointer to the location to which to copy the endpoint description.
- Returns
- True if the description was copied to result, or false if the endpoint is not active.
| EmberEUI64 emberGetEui64 | ( | void |
|
) |
Returns the EUI64 ID of the local node.
- Returns
- The 64-bit ID.
| void emberGetExtendedPanId | ( | uint8_t * |
resultLocation
|
) |
Fetches a node's 8 byte Extended PAN identifier. If this is called when a device is not currently on a network (see emberNetworkState ), the Extended PAN ID returned will be an invalid value.
| uint8_t emberGetInitialNeighborOutgoingCost | ( | void |
|
) |
Gets neighbor's initial outgoing link cost.
- Returns
- The default cost associated with new neighbor's outgoing links. NOTE: There is no EZSP version of this function yet.
| uint8_t emberGetMaxNwkRetries | ( | void |
|
) |
Get max number of NWK retries.
Returns the maximum number of NWK retries that will be attempted
- Returns
- uint8_t Max NWK retries
| EmberStatus emberGetNeighbor | ( | uint8_t |
index,
|
| EmberNeighborTableEntry * |
result
|
||
| ) |
Copies a neighbor table entry to the structure that
result
points to. Neighbor table entries are stored in ascending order by node ID, with all unused entries at the end of the table. The number of active neighbors can be obtained using
emberNeighborCount()
.
- Parameters
-
indexThe index of a neighbor table entry. resultA pointer to the location to which to copy the neighbor table entry.
- Returns
- EMBER_ERR_FATAL if the index is greater or equal to the number of active neighbors, or if the device is an end device. Returns EMBER_SUCCESS otherwise.
| EmberStatus emberGetNetworkParameters | ( | EmberNetworkParameters * |
parameters
|
) |
Copies the current network parameters into the structure provided by the caller.
- Parameters
-
parametersA pointer to an EmberNetworkParameters value into which the current network parameters will be copied.
- Returns
-
An
EmberStatusvalue indicating the success or failure of the command.
| EmberNodeId emberGetNodeId | ( | void |
|
) |
Returns the 16-bit node ID of local node on the current logical network.
- Returns
- The 16-bit ID.
| EmberStatus emberGetNodeType | ( | EmberNodeType * |
resultLocation
|
) |
Copies the current node type into the location provided by the caller.
- Parameters
-
resultLocationA pointer to an EmberNodeType value into which the current node type will be copied.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| EmberPanId emberGetPanId | ( | void |
|
) |
Returns the local node's PAN ID of the current logical network.
- Returns
- A PAN ID.
| uint8_t emberGetPhyInterfaceCount | ( | void |
|
) |
Returns the number of PHY interfaces present.
- Returns
- The number of PHY interface(s).
| uint8_t emberGetRadioChannel | ( | void |
|
) |
Gets the radio channel to which a node is set on the current logical network. The possible return values depend on the radio in use. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
- Returns
- The current radio channel.
| EmberStatus emberGetRadioParameters | ( | uint8_t |
phyIndex,
|
| EmberMultiPhyRadioParameters * |
parameters
|
||
| ) |
Copies the current radio parameters into the structure provided by the caller.
- Parameters
-
phyIndexThe index of the PHY interface for radio parameters. - For 2.4 or Subghz only (switched) device, index will be ignored.
- For simultaneous dual radio, returns radio parameters based on the provided PHY index. parameters A pointer to an EmberMultiPhyRadioParameters value into which the current radio parameters will be copied.
- Returns
-
An
EmberStatusvalue indicating the success or failure of the command.
| int8_t emberGetRadioPower | ( | void |
|
) |
Gets the radio output power of the current logical network at which a node is operating. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit.
- Returns
- The current radio output power, in dBm.
| EmberStatus emberGetRouteTableEntry | ( | uint8_t |
index,
|
| EmberRouteTableEntry * |
result
|
||
| ) |
Copies a route table entry to the structure that the
result
points to. Unused route table entries have a destination of 0xFFFF. The route table size can be obtained via
emberRouteTableSize()
.
- Parameters
-
indexThe index of a route table entry. resultA pointer to the location to which to copy the route table entry.
- Returns
- EMBER_ERR_FATAL if the index is out of range or the device is an end device, and EMBER_SUCCESS otherwise.
| uint8_t emberGetRoutingShortcutThreshold | ( | void |
|
) |
Gets the routing shortcut threshold used to separate between directly using a neighbor vs. performing routing.
- Returns
- the routingShortcutThresh which takes one of the following values: 1, 3, 5, or 7.
| uint16_t emberGetTxPowerMode | ( | void |
|
) |
Returns the current configuration of boost power mode and alternate transmitter output.
- Returns
- The current TX power mode.
| bool emberIsHubConnected | ( | void |
|
) |
- Returns
- true if there is hub connectivity, false otherwise
| bool emberIsLocalEui64 | ( | EmberEUI64 |
eui64
|
) |
Determines whether
eui64
is the local node's EUI64 ID.
- Parameters
-
eui64An EUI64 ID.
- Returns
-
True if
eui64is the local node's ID, otherwise false.
| bool emberIsNodeIdValid | ( | EmberNodeId |
nodeId
|
) |
Determines whether
nodeId
is valid.
- Parameters
-
nodeIdA node ID.
- Returns
-
True if
nodeIdis valid, false otherwise.
| bool emberIsResetRejoiningNeighborsFCEnabled | ( | void |
|
) |
Checks if resetting the incoming FC for a rejoining neighbor is enabled.
- Parameters
-
void
- Returns
- ::True or False. NOTE: There is no EZSP version of this function yet.
| bool emberIsUpTimeLong | ( | void |
|
) |
- Returns
- true if device uptime is long, false otherwise
| EmberStatus emberLookupEui64ByNodeId | ( | EmberNodeId |
nodeId,
|
| EmberEUI64 |
eui64Return
|
||
| ) |
Returns the EUI64 that corresponds to the specified node ID. The EUI64 is found by searching through all stack tables for the specified node ID.
- Parameters
-
nodeIdThe short ID of the node to look up. eui64ReturnThe EUI64 of the node is copied here if it is known.
- Returns
-
An
EmberStatusvalue:
- EMBER_SUCCESS - eui64Return has been set to the EUI64 of the node.
- EMBER_ERR_FATAL - The EUI64 of the node is not known.
| EmberNodeId emberLookupNodeIdByEui64 | ( | EmberEUI64 |
eui64
|
) |
Returns the node ID that corresponds to the specified EUI64. The node ID is found by searching through all stack tables for the specified EUI64.
- Parameters
-
eui64The EUI64 of the node to look up.
- Returns
- The short ID of the node or EMBER_NULL_NODE_ID if the short ID is not known.
| uint8_t emberNeighborCount | ( | void |
|
) |
Returns the number of active entries in the neighbor table.
- Returns
- The number of active entries in the neighbor table.
| EmberNetworkStatus emberNetworkState | ( | void |
|
) |
Returns the current join status.
Returns a value indicating whether the node is joining, joined to, or leaving a network.
- Returns
- An EmberNetworkStatus value indicating the current join status.
| uint8_t emberNextZigbeeSequenceNumber | ( | void |
|
) |
Increments and returns the Zigbee sequence number.
- Returns
- The next Zigbee sequence number.
| EmberNodeId emberRadioGetNodeId | ( | void |
|
) |
Returns the 16-bit node ID of local node on the network it is currently tuned on.
- Returns
- The 16-bit ID.
| EmberPanId emberRadioGetPanId | ( | void |
|
) |
Returns the local node's PAN ID of the current radio network.
- Returns
- A PAN ID.
| EmberStatus emberRadioGetSchedulerPriorities | ( | EmberMultiprotocolPriorities * |
priorities
|
) |
API used to get current zigbee priorities being used in multiprotocol applications. See UG305, the Dynamic Multiprotocol User Guide for more info on recommended priorities and discussion regarding interactivity with other stacks.
| void emberRadioNeedsCalibratingHandler | ( | void |
|
) |
The radio calibration callback function.
The Voltage Controlled Oscillator (VCO) can drift with temperature changes. During every call to emberTick() , the stack will check to see if the VCO has drifted. If the VCO has drifted, the stack will call emberRadioNeedsCalibratingHandler() to inform the application that it should perform calibration of the current channel as soon as possible. Calibration can take up to 150 ms. The default callback function implementation provided here performs the calibration immediately. The application can define its own callback by defining ::EMBER_APPLICATION_HAS_CUSTOM_RADIO_CALIBRATION_CALLBACK in its CONFIGURATION_HEADER. It can then failsafe any critical processes or peripherals before calling emberCalibrateCurrentChannel() . The application must call emberCalibrateCurrentChannel() in response to this callback to maintain expected radio performance.
| void emberResetRejoiningNeighborsFC | ( | bool |
reset
|
) |
Indicates whether a rejoining neighbor's incoming FC should be reset.
- Parameters
-
resetTrue or False.
- Returns
- ::void NOTE: There is no EZSP version of this function yet.
| uint8_t emberRouteTableSize | ( | void |
|
) |
Returns the size of the route table.
- Returns
- The size of the route table.
| bool emberRtosIdleHandler | ( | uint32_t * |
idleTimeMs
|
) |
A callback to allow the application to manage idling the MCU.
- Parameters
-
idleTimeMsThe time in millisecond the stack is allowed to idle.
- Returns
- True if the application is managing idling the MCU, false otherwise. If this function returns false, the stack will manage idling the MCU.
| void emberRtosStackWakeupIsrHandler | ( | void |
|
) |
A callback to request the application to wake up the stack task.
| EmberStatus emberSetBeaconClassificationParams | ( | EmberBeaconClassificationParams * |
param
|
) |
API used to set current beacon classification parameters.
| void emberSetDescriptorCapability | ( | uint8_t |
capability
|
) |
Sets the descriptor capability field of the node.
- Parameters
-
capabilityThe descriptor capability of the local node.
| void emberSetHubConnectivity | ( | bool |
connected
|
) |
sets the hub connectivity to be true or false the hub connectivity is then advertised in the beacons
| EmberStatus emberSetInitialNeighborOutgoingCost | ( | uint8_t |
cost
|
) |
Sets neighbor's initial outgoing link cost.
- Parameters
-
costThe new default cost.
- Returns
- EMBER_BAD_ARGUMENT if the cost is not any of 0, 1, 3, 5, or 7. Returns EMBER_SUCCESS otherwise NOTE: There is no EZSP version of this function yet.
| void emberSetLongUpTime | ( | bool |
hasLongUpTime
|
) |
sets the device uptime to be long or short the uptime is then advertised in the beacons
| void emberSetManufacturerCode | ( | uint16_t |
code
|
) |
Sets the manufacturer code to the specified value. The manufacturer code is one of the fields of the node descriptor.
- Parameters
-
codeThe manufacturer code for the local node.
| void emberSetMaximumIncomingTransferSize | ( | uint16_t |
size
|
) |
Sets the maximum incoming transfer size to the specified value. The maximum incoming transfer size is one of the fields of the node descriptor.
- Parameters
-
sizeThe maximum incoming transfer size for the local node.
| void emberSetMaximumOutgoingTransferSize | ( | uint16_t |
size
|
) |
Sets the maximum outgoing transfer size to the specified value. The maximum outgoing transfer size is one of the fields of the node descriptor.
- Parameters
-
sizeThe maximum outgoing transfer size for the local node.
| EmberStatus emberSetNodeId | ( | EmberNodeId |
nodeId
|
) |
Sets the short node ID of the node. Notice that it can only be set if the stack is in the INITAL state.
- Parameters
-
nodeIdSpecifies the short ID to be assigned to the node.
- Returns
- EMBER_SUCCESS if successful; an error code otherwise.
| void emberSetPowerDescriptor | ( | uint16_t |
descriptor
|
) |
Sets the power descriptor to the specified value. The power descriptor is a dynamic value, therefore this function should be called whenever the value changes.
- Parameters
-
descriptorThe new power descriptor for the local node.
| EmberStatus emberSetRadioChannel | ( | uint8_t |
channel
|
) |
Sets the channel to use for sending and receiving messages on the current logical network. For a list of available radio channels, see the technical specification for the RF communication module in your Developer Kit.
Note: When using this API, all devices on a network must use the same channel.
- Parameters
-
channelThe desired radio channel.
- Returns
-
An
EmberStatusvalue indicating the success or failure of the command.
| EmberStatus emberSetRadioPower | ( | int8_t |
power
|
) |
Sets the radio output power at which a node is to operate for the current logical network. Ember radios have discrete power settings. For a list of available power settings, see the technical specification for the RF communication module in your Developer Kit. Note that using this API on a running network will directly impact the established link qualities which the neighboring nodes have with the node on which it is called. This can lead to disruption of existing routes and erratic network behavior. Note that, if the requested power level is not available on a given radio, this function will use the next higher available power level.
- Parameters
-
powerA desired radio output power, in dBm.
- Returns
-
An
EmberStatusvalue indicating the success or failure of the command. Failure indicates that the requested power level is out of range.
| EmberStatus emberSetRoutingShortcutThreshold | ( | uint8_t |
costThresh
|
) |
Sets the routing shortcut threshold to directly use a neighbor instead of performing routing.
- Parameters
-
costThreshthe routing shortcut value that should be used to directly use a neighbor instead of performing routing.
- Returns
- ::return EMBER_BAD_ARGUMENT if the costThresh is not 1, 3, 5, 7 Returns EMBER_SUCCESS otherwise.
| EmberStatus emberSetTxPowerMode | ( | uint16_t |
txPowerMode
|
) |
Enables boost power mode and/or the alternate transmit path.
Boost power mode is a high-performance radio mode, which offers increased transmit power and receive sensitivity at the cost of an increase in power consumption. emberInit() calls this function using the power mode and transmitter output settings as specified in the MFG_PHY_CONFIG token (with each bit inverted so that the default token value of 0xffff corresponds to normal power mode and bi-directional RF transmitter output). The application only needs to call emberSetTxPowerMode() to use a power mode or transmitter output setting different than specified in the MFG_PHY_CONFIG token. After the initial call to emberSetTxPowerMode() , the stack will automatically maintain the specified power mode configuration across sleep/wake cycles.
- Parameters
-
txPowerModeSpecifies which transmit power mode options should be activated. This parameter should be set to one of the literal values described in stack/include/ember-types.h. Any power option not specified in the txPowerMode parameter will be deactivated.
- Returns
- EMBER_SUCCESS if successful; an error code otherwise.
| bool emberStackIsUp | ( | void |
|
) |
Indicates whether the stack is currently up.
Returns true if the stack is joined to a network and ready to send and receive messages. This reflects only the state of the local node; it does not indicate whether other nodes are able to communicate with this node.
- Returns
- True if the stack is up, false otherwise.
| uint8_t emberStackProfile | ( | void |
|
) |
Returns the stack profile of the network which the node has joined.
- Returns
- The stack profile.
| void emberStackStatusHandler | ( | EmberStatus |
status
|
) |
A callback invoked when the status of the stack changes. If the status parameter equals EMBER_NETWORK_UP , the emberGetNetworkParameters() function can be called to get the new network parameters. If any of the parameters are stored in nonvolatile memory by the application, the stored values should be updated.
The application is free to begin messaging after it receives the EMBER_NETWORK_UP status. However, routes discovered immediately after the stack comes up may be suboptimal because the routes are based on the neighbor table's information about two-way links with neighboring nodes, which is obtained from periodic ZigBee Link Status messages. It can take two or three link status exchange periods (of 16 seconds each) before the neighbor table has a good estimate of link quality to neighboring nodes. Therefore, the application may improve the quality of initially discovered routes by waiting after startup to give the neighbor table time to be populated.
- Parameters
| void emberStackTokenChangedHandler | ( | uint16_t |
tokenAddress
|
) |
A callback invoked to inform the application that a stack token has changed.
- Parameters
-
tokenAddressThe address of the stack token that has changed.
| uint8_t emberTreeDepth | ( | void |
|
) |
Returns the depth of the node in the network.
- Returns
- The current depth.
| EmberStatus emberWriteNodeData | ( | bool |
erase
|
) |
Writes node data to stack token.
- Parameters
-
boolIndicates whether the node type should be erased.
- Returns
- The status of the operation and an error code if unsuccessful.
Variable Documentation
| uint8_t emberEndpointCount |
The application must provide a definition for this variable.
| EmberEndpoint emberEndpoints[] |
If emberEndpointCount is nonzero, the application must provide descriptions for each endpoint.
This can be done either by providing a definition of emberEndpoints or by providing definitions of emberGetEndpoint() , emberGetEndpointDescription() and emberGetEndpointCluster() . Using the array is often simpler, but consumes large amounts of memory if emberEndpointCount is large.
If the application provides definitions for the three functions, it must define EMBER_APPLICATION_HAS_GET_ENDPOINT in its CONFIGURATION_HEADER.
| PGM uint8_t emberStackProfileId[] |
The application must provide a definition for this variable.