Message Fragmentation
Transmitting |
|
| EmberStatus | emberFragmentSendUnicast ( EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, EmberMessageBuffer payload, uint8_t maxFragmentSize) |
| bool | emberFragmentMessageSent ( EmberApsFrame *apsFrame, EmberMessageBuffer buffer, EmberStatus status) |
| void | emberFragmentMessageSentHandler ( EmberStatus status) |
Receiving |
|
| bool | emberFragmentIncomingMessage ( EmberApsFrame *apsFrame, EmberMessageBuffer payload) |
| void | emberFragmentTick (void) |
Initialization |
|
| void | ezspFragmentInit (uint16_t receiveBufferLength, uint8_t *receiveBuffer) |
|
Initialize variables and buffers used for sending and receiving long messages. This functions reads the values of ::EZSP_CONFIG_MAX_HOPS and ::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE. The application must set these values before calling this function.
|
|
Transmitting |
|
| EmberStatus | ezspFragmentSendUnicast ( EmberOutgoingMessageType type, uint16_t indexOrDestination, EmberApsFrame *apsFrame, uint8_t maxFragmentSize, uint16_t messageLength, uint8_t *messageContents) |
|
Sends a long message by splitting it into blocks. Only one long message can be sent at a time. Calling this function a second time aborts the first message.
|
|
| EmberStatus | ezspFragmentSourceRouteHandler (void) |
|
A callback invoked just before each block of the current long message is sent. If the message is to be source routed, the application must define this callback and call ezspSetSourceRoute() in it.
|
|
| bool | ezspFragmentMessageSent ( EmberApsFrame *apsFrame, EmberStatus status) |
|
The application must call this function at the start of its ezspMessageSentHandler(). If it returns true, the fragmentation code has handled the event and the application must not process it further.
|
|
| void | ezspFragmentMessageSentHandler ( EmberStatus status) |
|
The fragmentation code calls this application-defined handler when it finishes sending a long message.
|
|
Receiving |
|
| bool | ezspFragmentIncomingMessage ( EmberApsFrame *apsFrame, EmberNodeId sender, uint16_t *messageLength, uint8_t **messageContents) |
|
The application must call this function at the start of its ezspIncomingMessageHandler(). If it returns true, the fragmentation code has handled the message and the application must not process it further. When the final block of a long message is received, this function replaces the message with the reassembled long message and returns false so that the application processes it.
|
|
| void | ezspFragmentTick (void) |
|
Used by the fragmentation code to time incoming blocks. The application must call this function regularly.
|
|
Detailed Description
Splits long messages into smaller blocks for transmission and reassembles received blocks. See
fragment.h
for source code.
EMBER_FRAGMENT_WINDOW_SIZE controls how many blocks are sent at a time. EMBER_FRAGMENT_DELAY_MS controls the spacing between blocks.
To send a long message, the application calls emberFragmentSendUnicast() . The application must add a call to emberFragmentMessageSent() at the start of its emberMessageSentHandler() . If emberFragmentMessageSent() returns true, the fragmentation code has handled the event and the application must not process it further. The fragmentation code calls the application-defined emberFragmentMessageSentHandler() when it has finished sending the long message.
To receive a long message, the application must add a call to emberFragmentIncomingMessage() at the start of its emberIncomingMessageHandler() . If emberFragmentIncomingMessage() returns true, the fragmentation code has handled the message and the application must not process it further. The application must also call emberFragmentTick() regularly.
Fragmented message support for EZSP Hosts. Splits long messages into smaller blocks for transmission and reassembles received blocks. See fragment-host.c for source code.
::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE controls how many blocks are sent at a time. ::EZSP_CONFIG_FRAGMENT_DELAY_MS controls the spacing between blocks.
Before calling any of the other functions listed here, the application must call ezspFragmentInit() .
To send a long message, the application calls ezspFragmentSendUnicast() . The application must add a call to ezspFragmentMessageSent() at the start of its ezspMessageSentHandler(). If ezspFragmentMessageSent() returns true, the fragmentation code has handled the event and the application must not process it further. The fragmentation code calls the application-defined ezspFragmentMessageSentHandler() when it has finished sending the long message.
To receive a long message, the application must add a call to ezspFragmentIncomingMessage() at the start of its ezspIncomingMessageHandler(). If ezspFragmentIncomingMessage() returns true, the fragmentation code has handled the message and the application must not process it further. The application must also call ezspFragmentTick() regularly.
Function Documentation
| bool emberFragmentIncomingMessage | ( | EmberApsFrame * |
apsFrame,
|
| EmberMessageBuffer |
payload
|
||
| ) |
The application must call this function at the start of its emberIncomingMessageHandler() . If it returns true, the fragmentation code has handled the message and the application must not process it further. When the final block of a long message is received, this function replaces the message with the reassembled long message and returns false so that the application processes it.
- Parameters
-
apsFrameThe APS frame passed to emberIncomingMessageHandler() . payloadThe payload passed to emberIncomingMessageHandler() .
- Returns
- true if the incoming message was a block of an incomplete long message. The fragmentation code has handled the message so the application must return immediately from its emberIncomingMessageHandler() . Returns false if the incoming message was not part of a long message. The fragmentation code has not handled the message so the application must continue to process it. Returns false if the incoming message was a block that completed a long message. The fragmentation code replaces the message with the reassembled long message so the application must continue to process it.
| bool emberFragmentMessageSent | ( | EmberApsFrame * |
apsFrame,
|
| EmberMessageBuffer |
buffer,
|
||
| EmberStatus |
status
|
||
| ) |
The application must call this function at the start of its emberMessageSentHandler() . If it returns true, the fragmentation code has handled the event and the application must not process it further.
- Parameters
-
apsFrameThe APS frame passed to emberMessageSentHandler() . bufferThe buffer passed to emberMessageSentHandler() . statusThe status passed to emberMessageSentHandler() .
- Returns
- true if the sent message was a block of a long message. The fragmentation code has handled the event so the application must return immediately from its emberMessageSentHandler() . Returns false otherwise. The fragmentation code has not handled the event so the application must continue to process it.
| void emberFragmentMessageSentHandler | ( | EmberStatus |
status
|
) |
The fragmentation code calls this application-defined handler when it finishes sending a long message.
- Parameters
-
statusEMBER_SUCCESS if all the blocks of the long message were delivered to the destination, otherwise EMBER_DELIVERY_FAILED , EMBER_NO_BUFFERS , EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY .
| EmberStatus emberFragmentSendUnicast | ( | EmberOutgoingMessageType |
type,
|
| uint16_t |
indexOrDestination,
|
||
| EmberApsFrame * |
apsFrame,
|
||
| EmberMessageBuffer |
payload,
|
||
| uint8_t |
maxFragmentSize
|
||
| ) |
Sends a long message by splitting it into blocks. Only one long message can be sent at a time. Calling this function a second time aborts the first message.
- Parameters
-
typeSpecifies the outgoing message type. Must be one of EMBER_OUTGOING_DIRECT , EMBER_OUTGOING_VIA_ADDRESS_TABLE , or EMBER_OUTGOING_VIA_BINDING . indexOrDestinationDepending on the type of addressing used, this is either the EmberNodeId of the destination, an index into the address table, or an index into the binding table. apsFrameThe APS frame for the message. payloadThe long message to be sent. maxFragmentSizeThe message will be broken into blocks no larger than this.
- Returns
-
An EmberStatus value.
- EMBER_SUCCESS
- EMBER_MESSAGE_TOO_LONG
- EMBER_NO_BUFFERS
- EMBER_NETWORK_DOWN
- EMBER_NETWORK_BUSY
- EMBER_INVALID_CALL is returned if the payload length is zero or if the window size ( EMBER_FRAGMENT_WINDOW_SIZE ) is zero.
| void emberFragmentTick | ( | void |
|
) |
Used by the fragmentation code to time incoming blocks. The application must call this function regularly.
| bool ezspFragmentIncomingMessage | ( | EmberApsFrame * |
apsFrame,
|
| EmberNodeId |
sender,
|
||
| uint16_t * |
messageLength,
|
||
| uint8_t ** |
messageContents
|
||
| ) |
The application must call this function at the start of its ezspIncomingMessageHandler(). If it returns true, the fragmentation code has handled the message and the application must not process it further. When the final block of a long message is received, this function replaces the message with the reassembled long message and returns false so that the application processes it.
- Parameters
-
apsFrameThe APS frame passed to ezspIncomingMessageHandler(). senderThe sender passed to ezspIncomingMessageHandler(). messageLengthA pointer to the message length passed to ezspIncomingMessageHandler(). messageContentsA pointer to the message contents passed to ezspIncomingMessageHandler().
- Returns
- true if the incoming message was a block of an incomplete long message. The fragmentation code has handled the message so the application must return immediately from its ezspIncomingMessageHandler(). Returns false if the incoming message was not part of a long message. The fragmentation code has not handled the message so the application must continue to process it. Returns false if the incoming message was a block that completed a long message. The fragmentation code replaces the message with the reassembled long message so the application must continue to process it.
| void ezspFragmentInit | ( | uint16_t |
receiveBufferLength,
|
| uint8_t * |
receiveBuffer
|
||
| ) |
Initialize variables and buffers used for sending and receiving long messages. This functions reads the values of ::EZSP_CONFIG_MAX_HOPS and ::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE. The application must set these values before calling this function.
- Parameters
-
receiveBufferLengthThe length of receiveBuffer. Incoming messages longer than this will be dropped. receiveBufferThe buffer used to reassemble incoming long messages. Once the message is complete, this buffer will be passed back to the application by ezspFragmentIncomingMessage() .
| bool ezspFragmentMessageSent | ( | EmberApsFrame * |
apsFrame,
|
| EmberStatus |
status
|
||
| ) |
The application must call this function at the start of its ezspMessageSentHandler(). If it returns true, the fragmentation code has handled the event and the application must not process it further.
- Parameters
-
apsFrameThe APS frame passed to ezspMessageSentHandler(). statusThe status passed to ezspMessageSentHandler().
- Returns
- true if the sent message was a block of a long message. The fragmentation code has handled the event so the application must return immediately from its ezspMessageSentHandler(). Returns false otherwise. The fragmentation code has not handled the event so the application must continue to process it.
| void ezspFragmentMessageSentHandler | ( | EmberStatus |
status
|
) |
The fragmentation code calls this application-defined handler when it finishes sending a long message.
- Parameters
-
statusEMBER_SUCCESS if all the blocks of the long message were delivered to the destination, otherwise EMBER_DELIVERY_FAILED , EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY .
| EmberStatus ezspFragmentSendUnicast | ( | EmberOutgoingMessageType |
type,
|
| uint16_t |
indexOrDestination,
|
||
| EmberApsFrame * |
apsFrame,
|
||
| uint8_t |
maxFragmentSize,
|
||
| uint16_t |
messageLength,
|
||
| uint8_t * |
messageContents
|
||
| ) |
Sends a long message by splitting it into blocks. Only one long message can be sent at a time. Calling this function a second time aborts the first message.
- Parameters
-
typeSpecifies the outgoing message type. Must be one of EMBER_OUTGOING_DIRECT , EMBER_OUTGOING_VIA_ADDRESS_TABLE , or EMBER_OUTGOING_VIA_BINDING . indexOrDestinationDepending on the type of addressing used, this is either the EmberNodeId of the destination, an index into the address table, or an index into the binding table. apsFrameThe APS frame for the message. maxFragmentSizeThe message will be broken into blocks no larger than this. messageLengthThe length of the messageContents parameter in bytes. messageContentsThe long message to be sent.
- Returns
-
An EmberStatus value.
- EMBER_SUCCESS
- EMBER_MESSAGE_TOO_LONG
- EMBER_NETWORK_DOWN
- EMBER_NETWORK_BUSY
- EMBER_INVALID_CALL is returned if messageLength is zero or if the window size (::EZSP_CONFIG_FRAGMENT_WINDOW_SIZE) is zero.
| EmberStatus ezspFragmentSourceRouteHandler | ( | void |
|
) |
A callback invoked just before each block of the current long message is sent. If the message is to be source routed, the application must define this callback and call ezspSetSourceRoute() in it.
The application must define EZSP_APPLICATION_HAS_FRAGMENT_SOURCE_ROUTE_HANDLER in its configuration header if it defines this callback.
- Returns
- EMBER_SUCCESS if the source route has been set. Any other value will abort transmission of the current long message.
| void ezspFragmentTick | ( | void |
|
) |
Used by the fragmentation code to time incoming blocks. The application must call this function regularly.