#include < zll-types.h >

Data Fields

uint32_t bitmask
uint16_t freeNodeIdMin
uint16_t freeNodeIdMax
uint16_t myGroupIdMin
uint16_t freeGroupIdMin
uint16_t freeGroupIdMax
uint8_t rssiCorrection

Field Documentation

uint32_t EmberTokTypeStackZllData::bitmask
uint16_t EmberTokTypeStackZllData::freeGroupIdMax
uint16_t EmberTokTypeStackZllData::freeGroupIdMin
uint16_t EmberTokTypeStackZllData::freeNodeIdMax
uint16_t EmberTokTypeStackZllData::freeNodeIdMin
uint16_t EmberTokTypeStackZllData::myGroupIdMin
uint8_t EmberTokTypeStackZllData::rssiCorrection

The documentation for this struct was generated from the following file:
  • zll-types.h