EmberZNet debugging utilities.
EmberZNet debugging utilities.
See ember-debug.h
for source code.
#define emberDebugInit |
( |
|
port | ) |
do {} while (false) |
This function is obsolete and no longer required to initialize the debug system.
- Parameters
-
port | Ignored because the port used for debug communication is automatically determined for each platform. |
void emberDebugAssert |
( |
PGM_P |
filename, |
|
|
int |
linenumber |
|
) |
| |
Prints the filename and line number to the debug serial port.
- Parameters
-
filename | The name of the file where the assert occurred. |
linenumber | The line number in the file where the assert occurred. |
void emberDebugBinaryPrintf |
( |
PGM_P |
formatString, |
|
|
|
... |
|
) |
| |
Prints binary data to the debug channel.
This function does not use the normal printf format conventions. To print text debug messages, use emberDebugPrintf(). The format string must contain only these conversion specification characters:
- B - uint8_t value.
- W - uint16_t value, printed least significant byte first.
- D - uint32_t value, printed least significant byte first.
- F - pointer to null terminated string in Flash (PGM_P).
- xxxp - pointer to RAM, length is xxx (max 255).
- lp - pointer to RAM, length is uint8_t argument.
- xxxf - pointer to Flash (PGM_P), length is xxx (max 255).
- lf - pointer to Flash (PGM_P), length is uint8_t argument.
- b - EmberMessageBuffer.
Examples:
1 emberDebugBinaryPrintf("BWD", status, panId, channelMask);
2 emberDebugBinaryPrintf("F8p", "string example", eui64);
3 emberDebugBinaryPrintf("lp64fb", length, bytes, dataTable, buffer);
- Parameters
-
formatString | A string of conversion specification characters describing the arguments to be printed. |
... | The arguments to be printed. |
Prints an EmberStatus
return code to the serial port.
- Parameters
-
code | The EmberStatus code to print. |
void emberDebugMemoryDump |
( |
uint8_t * |
start, |
|
|
uint8_t * |
end |
|
) |
| |
Prints the contents of RAM to the debug serial port.
- Parameters
-
start | The start address of the block of RAM to dump. |
end | The end address of the block of RAM to dump (address of the last byte). |
void emberDebugPrintf |
( |
PGM_P |
formatString, |
|
|
|
... |
|
) |
| |
Prints text debug messages.
- Parameters
-
formatString | Takes the following: |
%% | Percent sign |
%c | Single-byte char |
%s | RAM string |
%p | Flash string (does not follow the printf standard) |
%u | Two-byte unsigned decimal |
%d | Two-byte signed decimal |
%x, %%2x, %%4x | 1-, 2-, 4-byte hex value (always 0 padded; does not follow the printf standard) |
bool emberDebugReportOff |
( |
void |
| ) |
|
Turns off all debug output.
- Returns
- The current state (true for on, false for off).
void emberDebugReportRestore |
( |
bool |
state | ) |
|
Restores the state of the debug output.
- Parameters
-
state | The state returned from emberDebugReportOff(). This is done so that debug output is not blindly turned on. |
void emDebugSendVuartMessage |
( |
uint8_t * |
buff, |
|
|
uint8_t |
len |
|
) |
| |
Sends VUART data out the debug channel.
- Parameters
-
buff | A pointer to the data to send. |
len | The length of the data to send. |