Ring Buffer#
API and Callbacks for the Ring Buffer Component.
This component manages a ring buffer of binary entries. Each entry has a 1- or 2-byte length field that is recorded to manage the buffer. This ring buffer can be used by multiple entities as the buffer space for the ring buffer is allocated by the caller.
Modules#
API#
Initialize the ring buffer struct based on data passed. widLengthField determines whether the ring buffer uses 1 or 2 byte length fields for entry. wideLengthField = false uses 1 byte length, wideLengthField = true uses 2 byte lengths. All entries in the same ring buffer utilze the same size length field. Different ring buffers may use differnt sizes.
Add an entry in the ring buffer.
Retrieve data from the specified entry. Returns the entry's total size in value pointed to by returnEntryTotalSize. The amount of data returned is written to the pointer returnDataSize. This allows for the caller to get the entry's total size at the same time they are able to grab a chunk of the entry up to some limit.
Get the last entry of the ring buffer.
Initialize the iterator to the first entry in the ring buffer. You may immediately call emberAfPluginRingBufferGetEntryByIterator() after this function is called.
Iterate to next entry in ring buffer.
Similar to emberAfPluginRingBufferGetEntryByEntryNumber().
Update a ring buffer entry by passing in the iterator.
Append an entry to end of the ring buffer.
Typedefs#
Macros#
API Documentation#
emberAfPluginRingBufferInitStruct#
EmberStatus emberAfPluginRingBufferInitStruct (EmberRingBuffer *ringBufferStruct, bool wideLengthField, EmberAfPluginRingBufferDeleteFunction *deleteCallback, uint8_t *dataPtr)
Initialize the ring buffer struct based on data passed. widLengthField determines whether the ring buffer uses 1 or 2 byte length fields for entry. wideLengthField = false uses 1 byte length, wideLengthField = true uses 2 byte lengths. All entries in the same ring buffer utilze the same size length field. Different ring buffers may use differnt sizes.
N/A | ringBufferStruct | Ver.: always |
N/A | wideLengthField | Ver.: always |
N/A | deleteCallback | Ver.: always |
N/A | dataPtr | Ver.: always |
Returns
EmberStatus status code
82
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferAddEntry#
EmberStatus emberAfPluginRingBufferAddEntry (EmberRingBuffer *ring, uint8_t *dataToAdd, uint16_t dataToAddSize)
Add an entry in the ring buffer.
N/A | ring | Ver.: always |
N/A | dataToAdd | Ver.: always |
N/A | dataToAddSize | Ver.: always |
Returns
EmberStatus status code
96
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferGetEntryByEntryNumber#
EmberStatus emberAfPluginRingBufferGetEntryByEntryNumber (EmberRingBuffer *ring, uint16_t entryNumber, uint16_t dataIndexInEntry, uint16_t *returnEntryTotalSize, uint16_t maxReturnSize, uint16_t *returnDataSize, uint8_t *returnData)
Retrieve data from the specified entry. Returns the entry's total size in value pointed to by returnEntryTotalSize. The amount of data returned is written to the pointer returnDataSize. This allows for the caller to get the entry's total size at the same time they are able to grab a chunk of the entry up to some limit.
N/A | ring | numbering starts from 0 |
N/A | entryNumber | may be set to NULL, in which case no return data is written. |
N/A | dataIndexInEntry | does not include the entry's length overhead, which the caller shouldn't care about anyway. |
N/A | returnEntryTotalSize | |
N/A | maxReturnSize | |
N/A | returnDataSize | |
N/A | returnData |
Returns
EmberStatus status code
115
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferGetLastEntry#
EmberStatus emberAfPluginRingBufferGetLastEntry (EmberRingBuffer *ring, uint16_t dataIndexInEntry, uint16_t *returnEntryTotalSize, uint16_t maxReturnSize, uint16_t *returnDataSize, uint8_t *returnData)
Get the last entry of the ring buffer.
N/A | ring | Ver.: always |
N/A | dataIndexInEntry | Ver.: always |
N/A | returnEntryTotalSize | Ver.: always |
N/A | maxReturnSize | Ver.: always |
N/A | returnDataSize | Ver.: always |
N/A | returnData | Ver.: always |
Returns
EmberStatus status code
134
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferInitIterator#
EmberStatus emberAfPluginRingBufferInitIterator (EmberRingBuffer *ring)
Initialize the iterator to the first entry in the ring buffer. You may immediately call emberAfPluginRingBufferGetEntryByIterator() after this function is called.
N/A | ring | Ver.: always |
Returns
EmberStatus status code
150
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferIteratorNextEntry#
EmberStatus emberAfPluginRingBufferIteratorNextEntry (EmberRingBuffer *ring)
Iterate to next entry in ring buffer.
N/A | ring | Ver.: always |
Returns
EmberStatus status code
Note
Return EMBER_OPERATION_IN_PROGRESS if there are more items left to iterate through. Returns EMBER_SUCCESS on reaching the last item, and the iterator is marked invalid (needs to be initialized again). Returns EMBER_INVALID_CALL if the iterator has not been initialized. An iterator can also be marked invalid if the ring buffer has deleted the entry that the iterator was currently on.
166
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferGetEntryByIterator#
EmberStatus emberAfPluginRingBufferGetEntryByIterator (EmberRingBuffer *ring, uint16_t dataIndexInEntry, uint16_t *returnEntryTotalSize, uint16_t maxReturnSize, uint16_t *returnDataSize, uint8_t *returnData)
Similar to emberAfPluginRingBufferGetEntryByEntryNumber().
N/A | ring | Ver.: always |
N/A | dataIndexInEntry | Ver.: always |
N/A | returnEntryTotalSize | Ver.: always |
N/A | maxReturnSize | Ver.: always |
N/A | returnDataSize | Ver.: always |
N/A | returnData | Ver.: always |
Returns
EmberStatus status code
Note
The iterator must have already been initialized
182
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferUpdateEntryByIterator#
EmberStatus emberAfPluginRingBufferUpdateEntryByIterator (EmberRingBuffer *ring, uint16_t dataIndexInEntry, uint8_t *updatedData, uint16_t updatedDataLength)
Update a ring buffer entry by passing in the iterator.
N/A | ring | Ver.: always |
N/A | dataIndexInEntry | Ver.: always |
N/A | updatedData | Ver.: always |
N/A | updatedDataLength | Ver.: always |
Returns
EmberStatus status code
199
of file app/framework/plugin/ring-buffer/ring-buffer.h
emberAfPluginRingBufferAppendLastEntry#
EmberStatus emberAfPluginRingBufferAppendLastEntry (EmberRingBuffer *ring, uint8_t *dataToAdd, uint16_t dataToAddSize)
Append an entry to end of the ring buffer.
N/A | ring | Ver.: always |
N/A | dataToAdd | Ver.: always |
N/A | dataToAddSize | Ver.: always |
Returns
EmberStatus status code
213
of file app/framework/plugin/ring-buffer/ring-buffer.h
Typedef Documentation#
EmberAfPluginRingBufferDeleteFunction#
typedef void() EmberAfPluginRingBufferDeleteFunction(uint16_t entryNumber, uint16_t entrySize) (uint16_t entryNumber, uint16_t entrySize)
41
of file app/framework/plugin/ring-buffer/ring-buffer.h
Macro Definition Documentation#
EMBER_AF_PLUGIN_RING_BUFFER_WIDE_LENGTH_ENTRY_OVERHEAD#
#define EMBER_AF_PLUGIN_RING_BUFFER_WIDE_LENGTH_ENTRY_OVERHEADValue:
2
35
of file app/framework/plugin/ring-buffer/ring-buffer.h
EMBER_AF_PLUGIN_RING_BUFFER_NARROW_LENGTH_ENTRY_OVERHEAD#
#define EMBER_AF_PLUGIN_RING_BUFFER_NARROW_LENGTH_ENTRY_OVERHEADValue:
1
36
of file app/framework/plugin/ring-buffer/ring-buffer.h
EMBER_AF_PLUGIN_RING_BUFFER_MAX_LENGTH_ENTRY_OVERHEAD#
#define EMBER_AF_PLUGIN_RING_BUFFER_MAX_LENGTH_ENTRY_OVERHEADValue:
EMBER_AF_PLUGIN_RING_BUFFER_WIDE_LENGTH_ENTRY_OVERHEAD
38
of file app/framework/plugin/ring-buffer/ring-buffer.h