ZLL Level Control Server#
API and Callbacks for the ZLL Level Control Cluster Server Component.
Silicon Labs implementation of the original Zigbee Light Link profile enhancements to the Level Control server cluster. The component is only intended to assist with debugging, as the implemented callbacks simply parse requests from the Identify client and blink LEDs. Before production, this component should be replaced with code that acts on the requests in an appropriate way. Note that the extensions do not now require Touchlink commissioning to be used, and that the commands may now be required by other device types, such as Lighting and Occupancy.
API#
emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions(const EmberAfClusterCommand *cmd)
bool
emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop(uint8_t endpoint, uint8_t commandId)
Macros#
API Documentation#
emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions#
EmberAfStatus emberAfPluginZllLevelControlServerMoveToLevelWithOnOffZllExtensions (const EmberAfClusterCommand *cmd)
Parameters
N/A | cmd |
Definition at line
48
of file app/framework/plugin/zll-level-control-server/zll-level-control-server.h
emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop#
bool emberAfPluginZllLevelControlServerIgnoreMoveToLevelMoveStepStop (uint8_t endpoint, uint8_t commandId)
Parameters
N/A | endpoint | |
N/A | commandId |
Definition at line
49
of file app/framework/plugin/zll-level-control-server/zll-level-control-server.h
Macro Definition Documentation#
EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MINIMUM_LEVEL#
#define EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MINIMUM_LEVELValue:
0x01
Definition at line
40
of file app/framework/plugin/zll-level-control-server/zll-level-control-server.h
EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MAXIMUM_LEVEL#
#define EMBER_AF_PLUGIN_ZLL_LEVEL_CONTROL_SERVER_MAXIMUM_LEVELValue:
0xFE
Definition at line
41
of file app/framework/plugin/zll-level-control-server/zll-level-control-server.h