Tunneling Server#
API and Callbacks for the Tunneling Cluster Server Component.
Silicon Labs implementation of Tunneling server cluster. This component requires extending to integrate the software that processes the tunneled data. Note if the maximum transfer size requires fragmentation, manually include the Fragmentation plugin and configure it to support the tunnel data size. Additionally, the component uses the address table to communicate with clients, so you must manually configure the address table size so that it accommodates active tunnels managed by this component as well as any other entries created during normal operation. The Tunneling cluster test specification suggests that implementations support the test protocol (protocol id 199, manufacturer code 0xFFFF). If you do not support it, you need some other means of proving two way communications works and is verifiable. If test protocol support is enabled, the component automatically handles requests for the test protocol and these messages will not fall through to the application.
Modules#
API#
Transfer data to a client through a tunneling cluster tunnel.
Toggle a "server busy" status for running as a test harness.
Clean up a tunneling cluster tunnel.
API Documentation#
emberAfPluginTunnelingServerTransferData#
EmberAfStatus emberAfPluginTunnelingServerTransferData (uint16_t tunnelIndex, uint8_t *data, uint16_t dataLen)
Transfer data to a client through a tunneling cluster tunnel.
N/A | tunnelIndex | The identifier of the tunnel through which to send data. |
N/A | data | The buffer containing the raw octets of data. |
N/A | dataLen | The length in octets of data. |
This function transfers data to a client through a tunnel. The tunneling server plugin will send data to the endpoint on the node that opened the given tunnel.
Returns
EMBER_ZCL_STATUS_SUCCESS Indicates if data was sent, EMBER_ZCL_STATUS_FAILURE if an error occurred, or EMBER_ZCL_STATUS_NOT_FOUND if the tunnel does not exist.
70
of file app/framework/plugin/tunneling-server/tunneling-server.h
emberAfPluginTunnelingServerToggleBusyCommand#
void emberAfPluginTunnelingServerToggleBusyCommand (void)
Toggle a "server busy" status for running as a test harness.
N/A |
This function sets the server into a busy state, where it will respond to all request tunnel commands with a busy status. NOTE: existing tunnels will continue to operate normally.
81
of file app/framework/plugin/tunneling-server/tunneling-server.h
emberAfPluginTunnelingServerCleanup#
void emberAfPluginTunnelingServerCleanup (uint8_t tunnelId)
Clean up a tunneling cluster tunnel.
N/A | tunnelId | The identifier of the tunnel to clean up. |
This function cleans up all states associated with a tunnel. The tunneling server plugin will not send the close notification command.
91
of file app/framework/plugin/tunneling-server/tunneling-server.h
Macro Definition Documentation#
ZCL_TUNNELING_CLUSTER_INVALID_TUNNEL_ID#
#define ZCL_TUNNELING_CLUSTER_INVALID_TUNNEL_IDValue:
0xFFFF
46
of file app/framework/plugin/tunneling-server/tunneling-server.h
ZCL_TUNNELING_CLUSTER_UNUSED_MANUFACTURER_CODE#
#define ZCL_TUNNELING_CLUSTER_UNUSED_MANUFACTURER_CODEValue:
0xFFFF
47
of file app/framework/plugin/tunneling-server/tunneling-server.h
CLOSE_INITIATED_BY_CLIENT#
#define CLOSE_INITIATED_BY_CLIENTValue:
true
48
of file app/framework/plugin/tunneling-server/tunneling-server.h
CLOSE_INITIATED_BY_SERVER#
#define CLOSE_INITIATED_BY_SERVERValue:
false
49
of file app/framework/plugin/tunneling-server/tunneling-server.h