EZ Mode#

Callbacks for EZ Mode Component.

Callbacks#

void

Client complete.

Callbacks Documentation#

sl_zigbee_af_ezmode_commissioning_client_complete_cb#

void sl_zigbee_af_ezmode_commissioning_client_complete_cb (uint8_t bindingIndex)

Client complete.

Parameters
N/AbindingIndex

The binding index that was created or ::SL_ZIGBEE_NULL_BINDING if an error occurred. Ver.: always

This function is called by the EZ Mode Commissioning plugin when client commissioning completes.


Definition at line 118 of file app/framework/plugin/ezmode-commissioning/ez-mode.h