Multirail Demo#

Callbacks for Multirail Demo Component.

Callbacks#

void
sl_zigbee_af_multirail_demo_rail_event_cb(RAIL_Handle_t handle, RAIL_Events_t events)

A callback called whenever a secondary instance RAIL event occurs.

void

A callback called to initialize the green power TX queue.

Callbacks Documentation#

sl_zigbee_af_multirail_demo_rail_event_cb#

void sl_zigbee_af_multirail_demo_rail_event_cb (RAIL_Handle_t handle, RAIL_Events_t events)

A callback called whenever a secondary instance RAIL event occurs.

Parameters
[in]handle

A handle for a RAIL instance.

[in]events

A bit mask of RAIL events (full list in rail_types.h)


Definition at line 117 of file app/framework/plugin/multirail-demo/multirail-demo.h

sl_zigbee_multirail_gp_tx_queue_init#

void sl_zigbee_multirail_gp_tx_queue_init (void )

A callback called to initialize the green power TX queue.

Parameters
N/A

Definition at line 123 of file app/framework/plugin/multirail-demo/multirail-demo.h