sl_bt_evt_cte_receiver_dtm_iq_reportCTE Receiver

IQ sample report from DTM CTE packets.

Data Structures

struct  sl_bt_evt_cte_receiver_dtm_iq_report_s
 Data structure of the dtm_iq_report event.
 

Macros

#define sl_bt_evt_cte_receiver_dtm_iq_report_id   0x024500a0
 Identifier of the dtm_iq_report event.
 

Detailed Description

IQ sample report from DTM CTE packets.


Data Structure Documentation

◆ sl_bt_evt_cte_receiver_dtm_iq_report_s

struct sl_bt_evt_cte_receiver_dtm_iq_report_s

Data structure of the dtm_iq_report event.

Data Fields
uint16_t status

Status of CTE IQ sampling

uint8_t channel

The channel on which the CTE packet was received

int8_t rssi

RSSI in the received CTE packet. Unit: dBm

uint8_t rssi_antenna_id

The ID of the antenna on which RSSI was measured

uint8_t cte_type

The CTE type

  • 0: AoA CTE response
  • 1: AoD CTE response with 1us slots
  • 2: AoD CTE response with 2us slots
uint8_t slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each
  • 2: Switching and sampling slots are 2 us each
uint16_t event_counter

The event counter of the periodic advertising train or the connection

uint8array samples

IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...)