Data structure of the node_failed event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_node_failed_s::elem_index
Server model element index
Definition at line
17503
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
address#
uint16_t sl_btmesh_evt_fw_dist_server_node_failed_s::address
Address of the Update Server
Definition at line
17504
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_phase#
uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::update_phase
Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Update Phase of the Update Server. 0xa if not known yet.
Definition at line
17505
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_status#
uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::update_status
Enum sl_btmesh_fw_update_server_update_status_t. Last Update Status message received from the Update Server
Definition at line
17509
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
mbt_status#
uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::mbt_status
Last status code received from the MBT Server. 0xa if not known yet.
Definition at line
17513
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
progress#
uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::progress
0-100, percentage of BLOB Transfer octets delivered and confirmed
Definition at line
17515
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint8_t sl_btmesh_evt_fw_dist_server_node_failed_s::fw_index
Index of the firmware being updated
Definition at line
17517
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h