Data structure of the nodes_added event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_added_s::elem_index

Server model element index


Definition at line 17279 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_added_s::client_address

Address of the Distribution Client


Definition at line 17280 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

total_nodes#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_added_s::total_nodes

Total number of nodes now on the list


Definition at line 17281 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

num_added_nodes#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_added_s::num_added_nodes

Number of nodes added


Definition at line 17282 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

added_nodes#

uint8array sl_btmesh_evt_fw_dist_server_nodes_added_s::added_nodes

Address - firmware index pairs that were added


Definition at line 17283 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h