Data structure of the resume_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::elem_index
Server model element index
Definition at line
17733
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::client_address
Address of the Distribution Client
Definition at line
17734
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
group_address#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::group_address
Group address to use for the distribution
Definition at line
17735
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
app_index#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::app_index
Appkey index to use for the distribution
Definition at line
17736
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ttl#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::ttl
TTL to use for the distribution
Definition at line
17737
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
update_policy#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::update_policy
Update Policy to use for the distribution
Definition at line
17738
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_index#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::fw_index
Distribution Server's Firmware Image List Index of the image to transfer
Definition at line
17739
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
timeout_base#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::timeout_base
Timeout Base to use for the distribution
Definition at line
17741
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_mode#
uint16_t sl_btmesh_evt_fw_dist_server_resume_req_s::transfer_mode
BLOB Transfer Mode to use for transferring the image
Definition at line
17742
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h