Data structure of the upload_oob_start_uri event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::elem_index
Server model element index
Definition at line
17612
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::client_address
Address of the Distribution Client
Definition at line
17613
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uri#
uint8array sl_btmesh_evt_fw_dist_server_upload_oob_start_uri_s::uri
URI to use for retrieving a new firmware image
Definition at line
17614
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h