Data structure of the mode_updated event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_server_mode_updated_s::destination_address

Message destination address if triggered by a message, 0 otherwise.


Definition at line 13948 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_server_mode_updated_s::elem_index

Index of the element where the update happened


Definition at line 13950 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_lc_server_mode_updated_s::client_address

Message source address if triggered by a message, 0 otherwise.


Definition at line 13952 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_server_mode_updated_s::appkey_index

Message appkey index if triggered by a message, 0xFFFF otherwise.


Definition at line 13954 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

mode_value#

uint8_t sl_btmesh_evt_lc_server_mode_updated_s::mode_value

The value the LC Mode state is being set to.


Definition at line 13956 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

manual_override#

uint8_t sl_btmesh_evt_lc_server_mode_updated_s::manual_override

Light Control Mode state can be set to zero by a binding from Light Lightness Linear when it is modified by an action from the application or a Light Lightness Client command. In this case, the parameter is set to 0x01. In all other cases, this parameter is zero. For example, when LC Mode is modified by the application or by a LC Client command, this parameter will be set to 0.


Definition at line 13958 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h