Data structure of the state_updated event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_lc_server_state_updated_s::elem_index
Index of the element where the update happened
Definition at line
14147
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
state#
uint8_t sl_btmesh_evt_lc_server_state_updated_s::state
The updated value of the LC state
Definition at line
14148
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transition_time#
uint32_t sl_btmesh_evt_lc_server_state_updated_s::transition_time
Transition time defined for the current LC state.
Definition at line
14149
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h