Data structure of the changed_ivupdate_state event.

Public Attributes#

uint32_t
uint8_t

Public Attribute Documentation#

iv_index#

uint32_t sl_btmesh_evt_node_changed_ivupdate_state_s::iv_index

Current IV index


Definition at line 717 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

state#

uint8_t sl_btmesh_evt_node_changed_ivupdate_state_s::state

Indicates whether the IV index update is ongoing (1) or not (0).


Definition at line 718 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h