Data structure of the key_removed event.
Public Attribute Documentation#
type#
uint8_t sl_btmesh_evt_node_key_removed_s::type
Type of the removed key. Values are as follows:
0x00: Network key
0x01: Application key
Definition at line
755
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
index#
uint16_t sl_btmesh_evt_node_key_removed_s::index
Key index of the removed key
Definition at line
758
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
netkey_index#
uint16_t sl_btmesh_evt_node_key_removed_s::netkey_index
Network key index to which the application key is bound, which is ignored for network keys
Definition at line
759
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h