Data structure of the oob_auth_request event.

Public Attributes#

uint8_t

Public Attribute Documentation#

output#

uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output

Zero for static data, non-zero for output


Definition at line 2411 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

output_action#

uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output_action

Enum sl_btmesh_node_oob_output_action_t. Output action type. Ignored for Static.


Definition at line 2412 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

output_size#

uint8_t sl_btmesh_evt_prov_oob_auth_request_s::output_size

Size of output data. Ignored for Static.


Definition at line 2414 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_oob_auth_request_s::uuid

UUID of the device


Definition at line 2415 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h