Data structure of the oob_display_input event.

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_oob_display_input_s::uuid

UUID of the device


Definition at line 2437 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

input_action#

uint8_t sl_btmesh_evt_prov_oob_display_input_s::input_action

Enum sl_btmesh_node_oob_input_action_t. Input action type


Definition at line 2438 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

input_size#

uint8_t sl_btmesh_evt_prov_oob_display_input_s::input_size

Number of digits or characters


Definition at line 2440 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

data#

uint8array sl_btmesh_evt_prov_oob_display_input_s::data

Raw 16-byte array


Definition at line 2441 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h