Data structure of the uri event.

Public Attributes#

uint32_t

Public Attribute Documentation#

hash#

uint32_t sl_btmesh_evt_prov_uri_s::hash

URI hash. If a Provisioner is provisioning a device which supports out-of-band provisioning and has supplied a URI hash value in its Unprovisioned Device beacon, the Provisioner should check whether the hash matches this value.


Definition at line 2485 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

data#

uint8array sl_btmesh_evt_prov_uri_s::data

Raw URI data, formatted as specified in Bluetooth Core System Supplement v6.


Definition at line 2490 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h