Data structure of the get_column_request event.
Public Attribute Documentation#
server_address#
uint16_t sl_btmesh_evt_sensor_server_get_column_request_s::server_address
Destination server address
Definition at line
11686
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_sensor_server_get_column_request_s::elem_index
Server model element index
Definition at line
11687
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_sensor_server_get_column_request_s::client_address
Source client model address
Definition at line
11688
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_sensor_server_get_column_request_s::appkey_index
The application key index to use
Definition at line
11689
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
flags#
uint8_t sl_btmesh_evt_sensor_server_get_column_request_s::flags
No flags defined currently
Definition at line
11690
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_sensor_server_get_column_request_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.
Definition at line
11691
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
column_ids#
uint8array sl_btmesh_evt_sensor_server_get_column_request_s::column_ids
Raw value identifying a column
Definition at line
11694
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h