GPIO-Controlled Network Connection
This example demonstrates how to use a GPIO to control a network connection to a remote server. Once the network connection is open, data can be automatically streamed between Gecko OS and the remote server.
     
    
Features Demonstrated
- ioconn.* variables
 - gpio.alias variable
 
Method
     The Gecko OS
     
      ioconn
     
     feature makes it easy for an MCU, or blackbox electronic system with a serial output, to add network communication with a remote server. A GPIO is assigned as the
     
      ioconn.control_gpio
     
     . Toggling the ioconn control GPIO makes and breaks the network connection to the remote server.
    
     The remote server used in the demonstration is the Zentri test TCP echo server, located online at
     
      test.zentri.com
     
     . The TCP echo server simply echoes any messages back to the client.
    
A computer, connected via USB to the evaluation board, takes the part of the MCU host system.
To set the level of the ioconn control GPIO high, various techniques are possible. In this demonstration, a switch is used to connect a logic high (3.3V) to the ioconn control GPIO pin. In an actual implementation, the host system toggles the ioconn control GPIO.
     
    
This demonstration uses the user LED GPIOs on the module for the ioconn control and status GPIOs. The LEDs are configured so that:
- User LED1 turns on when the ioconn control GPIO is asserted
 - User LED2 turns on when a connection with the remote server is established
 
This demonstration works on a Gecko OS evaluation board.
Setup
Connect the switch between the IOC_CTRL and VDD_3V3. Sample pins are shown. Use the pins appropriate for your device and evaluation board:
|IOC_CTRL (LED 1) | VDD_3V3 | IOC_STATUS (LED2) |
| GPIO 22: Pin H2-10 | Pin H2-20| GPIO 21 |
Connect the module via USB to your computer and open a serial terminal console. See Getting Started .
The following assumes that the module is in the default state. To return to the default state, perform a factory reset .
Set up the local Wi-Fi network parameters.
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
Set up aliases for the ioconn variables.
For example:
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
Configure the ioconn variables.
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
Performing a GPIO-Controlled Host Connection
     When the
     
      IOC_CTRL
     
     GPIO is low, the
     
      stream_list
     
     command does not list any TCP client network stream:
    
> stream_list
! # Type  Info
    
     Assert the module
     
      IOC_CTRL
     
     GPIO by setting the switch to ON.
    
If all goes well, the module terminal console displays something like the following:
| Gecko OS Response | 
|---|
       
       | 
     
The stream_list command lists the new TCP client network stream:
> stream_list
! # Type  Info
# 0 TCPC  107.170.222.80:50007 (22316)
    
     While the
     
      IOC_CTRL
     
     GPIO is still asserted, send a message to the server:
    
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
| Gecko OS Response | 
|---|
       
       | 
     
Now check if a message has been received in reply:
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
| Gecko OS Response | 
|---|
       
       | 
     
The server's response echoes the message sent.
De-assert the ioconn control GPIO by setting the switch to OFF.
The Gecko OS response is similar to the following:
| Gecko OS Response | 
|---|
       
       | 
     
Once again, the stream_list command does not list any TCP client network stream:
> stream_list
! # Type  Info
    Using Stream Mode
A typical use of the GPIO Controlled Network Connection feature is to allow a device to stream data to and from a server. To demonstrate this, put the module in stream mode:
| Gecko OS commands | Comments | 
|---|---|
       
       | 
      
       
       | 
     
The module terminal console can no longer send commands to Gecko OS. Try typing at the terminal. There is no response. Characters you type are transparently streamed to the network, which is currently not connected. See Serial Interface, Stream Mode .
Now assert the ioconn control GPIO by setting the switch to on.
Gecko OS responds as follows:
| Gecko OS Response | 
|---|
       
       | 
     
All characters received from the remote server appear automatically on the console.
Now type some characters into the module terminal console. Typed characters are echoed (after round-trip network latency) by the Zentri test server.
Supporting Gecko OS Versions
- Gecko OS 4
 
Change Log
| Modified | Changes | 
|---|---|
| 2019-01-01 | Created |