TCP Server
tcp.server.auto_interface
Abbreviation
tc s i
Access
get/set
Description
Wireless interface used for the TCP server if auto-start is enabled.
If set to
default
, uses the interface specified in
network.default_interface
Arguments
<wlan/softap/default>
Default
default
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s i
R000009
default
Set example
> set tc s i softap
R000008
Set OK
tcp.server.auto_start
Abbreviation
tc s a
Access
get/set
Description
Enable/disable TCP server auto-start on bootup.
Arguments
<1|true|on/0|false|off>
where
-
0orfalseoroff: auto-start disabled -
1ortrueoron: auto-start enabled
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s a
R000003
0
Set example
> set tc s a true
R000008
Set OK
tcp.server.connected_gpio
Abbreviation
tc s c
Access
get/set
Description
The GPIO used to indicate whether a client is connected to the TCP server.
See also system.oob.gpio .
Arguments
<[GPIO#]/[-1]>
Default
-1
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s c
R000004
-1
Set example
> set tc s c 12
R000008
Set OK
tcp.server.data_gpio
Abbreviation
tc s d
Access
get/set
Description
The GPIO used to indicate whether a connected client has data available to read.
Note
: Disable by setting to -1.
See also system.oob.gpio .
Arguments
<GPIO#>
Default
-1
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s d
R000004
-1
Set example
> set tc s d 13
R000008
Set OK
tcp.server.idle_timeout
Abbreviation
tc s t
Access
get/set
Description
Maximum client idle time in seconds before the client is automatically disconnected.
Setting
tcp.server.idle_timeout
to
0
turns off timeout completely: TCP server does not disconnect idle clients.
Arguments
<seconds>
Default
60
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s t
R000004
60
Set example
> set tc s t 30
R000008
Set OK
tcp.server.max_clients
Abbreviation
tc s m
Access
get/set
Description
Specify maximum number of clients that may be simultaneously connected to the tcp server.
This variable applies only when
bus.mode
=
command
.
If
bus.mode
=
stream
, max TCP server clients = 1
Arguments
<max #> - maximum number of TCP server clients, valid range: 0-8.
where:
0
is a deprecated value. If
tcp.server.max_clients
=
0
and
bus.mode
=
command
, then max TCP server clients = 8
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> > get tc s m
0
Set example
> set tc s m 5
Set OK
tcp.server.port
Abbreviation
tc s p
Access
get/set
Description
TCP server port to listen on
Arguments
<port>
Default
3000
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s p
R000006
3000
Set example
> set tc s p 3001
R000008
Set OK
tcp.server.tls_cert
Abbreviation
tc s n
Access
get/set
Description
The server TLS CA certificate filename.
Arguments
<filename>
Default
null
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s n
R000012
mycert.pem
Set example
> set tc s n mycert.pem
R000008
Set OK
tcp.server.tls_enabled
Abbreviation
tc s u
Access
get/set
Description
Enable server TLS certificate (used with auto_start option)
Arguments
<1|true|on/0|false|off>
where
-
0orfalseoroff: disabled -
1ortrueoron: enabled
Default
false
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s u
R000003
0
Set example
> set tc s u false
R000008
Set OK
tcp.server.tls_key
Abbreviation
tc s k
Access
get/set
Description
The server TLS certificate key filename.
Arguments
<filename>
Default
null
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s k
R000012
mycert.key
Set example
> set tc s k mycert.key
R000008
Set OK
tcp.server.tls_verify_peer
Abbreviation
tc s v
Access
get/set
Description
When this variable is set, a connecting client must provide a valid TLS certificate that the server validates. The client is disconnected if the provided certifcate is invalid.
Note : The tcp.server.tls_cert variable must be set if using this feature.
Arguments
<1|true|on/0|false|off>
where
-
0orfalseoroff: disabled -
1ortrueoron: enabled
Default
0
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Get example
> get tc s v
0
Set example
> set tc s v 1
Set OK