Sending a Secure SMTP Email
Set Up the Email and SMTP Variables
The first step is to set the email and SMTP variables with values depending on your SMTP email account.
| Gecko OS Commands | Description | 
|---|---|
       
        set email.name_address your@email.address set email.smtp.username your_user_name set email.smtp.password your_password set email.smtp.host your_smtp_host set email.smtp.port your_smtp_host_port
       
       | 
      
       
        Specify your email address Specify your user name. This may be same as your email address Specify your SMTP password Specify the SMTP host via which you send email Specify the SMTP host port. This is typically 587 for secure SMTP
       
       | 
     
     For example, if your email is
     
      fred@gmail.com
     
     :
    
set email.name_address  fred@gmail.com
set email.smtp.username  fred@gmail.com
set email.smtp.password s3cr3tFredword
set email.smtp.host  smtp.gmail.com
set email.smtp.port 587
    Set Maximum TLS version
This step is necessary only if the SMTP server requires it. You may need to set a maximum TLS version with the network.tls.version variable. For example:
set network.tls.version 10
    Set the CA Certificate for your Device
You may require a TLS certificate for your device.
Obtain the Certificate
     Obtain the certification in
     
      .pem
     
     format. For a discussion of certificates see the
     
      TLS Client app note
     
     .
    
Copy the Certificate to your Device
You can use the file_create command. For example:
file_create fred_ca_cert.pem 1569
-----BEGIN CERTIFICATE-----
d3RlLCBJbm...
...49cOSvkB5iy6
-----END_CERTIFICATE-----
    
     Copy the certificate text from
     
      -----BEGIN CERTIFICATE-----
     
     to
     
      -----END_CERTIFICATE-----
     
     .
    
Alternatively you can use the Silicon Labs Web App Files tab to drag and drop the certificate file.
See Gecko OS Web App, Files Tab .
Set the Network TLS CA Cert
Set the value of the the network.tls.ca_cert to the CA certificate file you have created. For example:
set network.tls.ca_cert fred_ca_cert.pem
    Configure Gmail to Support Sending Emails from Gecko OS
     In the case of the Google SMTP servers, you need to switch the Google mail
     
      Access for less secure apps
     
     setting on.
    
See https://www.google.com/settings/security/lesssecureapps .
Send the Email
To send the email using the command API, use the smtp_send command:
smtp_send <to email address> <email subject> <length of email content>
    To send the email using the Native API, use the SMTP API .
Supporting Gecko OS Versions
- Gecko OS 4
 
Change Log
| Modified | Changes | 
|---|---|
| 2019-01-01 | Created |