SPI Settings
spi.master.active_gpio
Abbreviation
     
      sp m g
     
    
Access
     
      get/set
     
    
Description
Specify the GPIO that is asserted when the module's SPI master bus is being accessed. At this time, any non-SPI peripheral signals connected to the SPI GPIOs should be set to high impedance.
Arguments
     
      <gpio #>
     
    
     
      Note
     
     : Set to
     
      -1
     
     to disable this feature, and free a GPIO assigned to this function.
    
Default
     
      -1
     
    
Properties
Gecko OS Kernel Plugin
Get example
> get sp m g
-1
    Set example
> set sp m g 9
Set OK
> get gp u
!  # Description
...
#  9 spi.master.active_gpio
...
    spi.master.active_level
Abbreviation
     
      sp m l
     
    
Access
     
      get/set
     
    
Description
Specify the asserted level for spi.master.active_gpio
Arguments
     
      <0/1>
     
    
Default
     
      1
     
    
Properties
Gecko OS Kernel Plugin
Get example
> get sp m l
1
    Set example
> set sp m l 0
Set OK