Broadcast
broadcast.data
Abbreviation
br d
Access
get/set
Description
A comma separated list of information fields to be periodically transmitted in a UDP packet or sent to a remote HTTP server. See the Broadcast UDP Packet application note.
Arguments
<csv list>
where
<csv list>
is a comma separated value list constructed from:
| List Item | Description |
|---|---|
| adcX | Current value of ADC X |
| bssid | wlan interface -> BSSID of the AP |
| channel | Wi-Fi radio channel |
| gpioX | Current state of GPIO X |
| ip | Current IP address |
| mac | wlan MAC address |
| rssi | wlan interface -> RSSI of the AP |
| ssid | wlan interface -> SSID of the AP |
| time | Gecko OS local time |
| uuid | Hardware ID |
| version | Firmware version |
| remote_terminal_port | inbound network port for the remote terminal |
Default
mac,bssid,channel,ip,ssid,rssi,remote_terminal_port,time,uuid,version
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get br d
R000033
mac,bssid,channel,version,gpio0
Set example
> set br d mac,bssid,channel
R000008
Set OK
broadcast.http.host
Abbreviation
br h h
Access
get/set
Description
When specified, periodically issue JSON formatted data to the specified host as an HTTP(S) post request. If null, the HTTP post function is disabled. The post may be to an unencrypted or HTTPS secure webserver. If a non-standard HTTP/HTTPS port is required, the port may be appended to the end of the URL, for example
myserver.com:3002
. The URL must be prefixed with
https://
for HTTPS secure connections on the default port 443.
Arguments
<http_host>
Default
Null
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get br h h
myhttpserver.com
Set OK
Set example
> set br h h myhttpserver.com
Set OK
Set example 2
> set br h h https://mysecureserver.com
Set OK
broadcast.interface
Abbreviation
br i
Access
get/set
Description
The default interface used to transmit informational packets.
If set to
default
, uses the interface specified in
network.default_interface
Arguments
<wlan/softap/default>
Default
default
Properties
Gecko OS Kernel Plugin
Get example
> get br i
R000006
wlan
Set example
> set br i softap
R000008
Set OK
broadcast.interval
Abbreviation
br t
Access
get/set
Description
The time between transmission of informational packets. Units are in seconds.
To disable both UDP and HTTP broadcast, set the interval to 0, except when the device is in web setup mode.
Periodic UDP broadcast is always enabled in web setup mode.
During web setup mode, if
broadcast.interval
=
0
then the broadcast period is
3
s. If broadcast.interval >
0
then broadcast period is the value of
broadcast.interval
.
During normal operation, if
broadcast.interval
=
0
then UDP and HTTP broadcast are disabled.
Arguments
<seconds>
Range: 0 - 65535
Default
10
Properties
Gecko OS Kernel Plugin
Get example
> get br t
R000004
10
Set example
> set br t 20
R000008
Set OK
broadcast.udp.ip
Abbreviation
br u a
Access
get/set
Description
Informational UDP packets are sent to this IP address.
To enable general UDP broadcast, set the IP address to 255.255.255.255 (default), i.e
set broadcast.udp.ip 255.255.255.255
To disable UDP broadcast, set the IP address to 0.0.0.0, i.e
set broadcast.udp.ip 0.0.0.0
Alternatively, set
broadcast.interval
to
0
to disable both UDP and HTTP broadcast.
Arguments
<IP address>
Default
255.255.255.255
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get br u a
R000017
255.255.255.255
Set example
> set br u a 192.168.1.255
R000008
Set OK
broadcast.udp.local_port
Abbreviation
br u l
Access
get/set
Description
Specifies the local port on which UDP broadcast transmits. It is mapped to the Source Port field on the UDP packet.
For legacy purposes, if the local port is set to
0
or
65535
, then the local port is set to
udp.broadcast.port
(i.e. the remote transmit port).
Arguments
<port>
Range
1-65534
Default
55555
Supported Platforms
- WGM160P
Get example
> get br u l
R000007
55555
Set example
> set br u l 50007
R000008
Set OK
broadcast.udp.remote_port
Abbreviation
br u p
Access
get/set
Description
Informational UDP packets are sent to this port.
Arguments
<port>
Default
55555
Properties
- takes effect immediately
Gecko OS Kernel Plugin
Get example
> get br u p
R000007
55555
Set example
> set br u p 50007
R000008
Set OK