Time
time.last_set
Abbreviation
     
      ti l
     
    
Access
     
      get
     
    
Description
Return the number of seconds (or milliseconds) since the time was set (either manually or via NTP ), or -1 if the time has never been set.
Get arguments
     
      [ms]
     
    
Default
     
      -
     
    
Gecko OS Kernel Plugin
Get example
> get ti l
R000005
239
    time.rtc
Abbreviation
     
      ti r
     
    
Access
     
      get/set
     
    
Description
     The local time. Read returns epoch seconds by default, or (optionally) epoch milliseconds or UTC. Write takes an
     
Get arguments
     
      [ms/utc]
     
    
Set arguments
     
      <epoch seconds>
     
    
Default
     
      -
     
    
Properties
- takes effect immediately
 
Gecko OS Kernel Plugin
Get example
> get ti r utc
R000029
2019-01-01-23T08:13:07.010248Z
    Set example
> set ti r 1395562166
R000008
Set OK
    time.uptime
Abbreviation
     
      ti u
     
    
Access
     
      get
     
    
Description
Returns the number of seconds (or milliseconds) since reset, guaranteed not to roll over in your lifetime!
Arguments
     
      [ms]
     
    
Default
     
      <varies>
     
    
Gecko OS Kernel Plugin
Get example
> get ti u ms
R000006
3578576
    time.zone
Abbreviation
     
      ti z
     
    
Access
     
      get/set
     
    
Description
Timezone offset from GMT in hours.
Arguments
     
      [+/-]H[:M]
     
     where H is an integer between 0 and 12, and M (if present) = 30
     
     Offset ranges from -12:30 to 12:30.
    
Default
     
      0
     
    
Properties
- takes effect immediately
 
Gecko OS Kernel Plugin
Get example
> get ti z
R000007
-4:30
    Set example
> set ti z -4:30
R000008
Set OK