mDNS
mdns.enabled
Abbreviation
md e
Access
get/set
Description
Enable the mDNS daemon (i.e. background process). The process is started when the configured interface is brought up (see mdns.interface ). If the network interface is already up when mDNS is enabled, bring the network interface down and up again to start mDNS (see network_down , network_up ). See Networking and Security, Network Discovery .
Note : When mDNS is enabled, .local domains are first attempted to be resolved using mDNS. If the attempt fails, standard DNS is then attempted.
Arguments
<1|true|on/0|false|off>
Default
1
Set example
> set mdns.enabled 1
Set OK
Get example
> get md e
1
mdns.interface
Abbreviation
md i
Access
get/set
Description
The network interface on which the mDNS daemon runs. See Networking and Security, Network Discovery .
Arguments
<default/softap/wlan>
Default
default
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Set example
> set mdns.interface wlan
Set OK
Get example
> get md i
wlan
mdns.name
Abbreviation
md n
Access
get/set
Description
The mDNS domain name of the module.
Note :
-
.localis appended to the name. See Networking and Security, Network Discovery . -
If the specified name conflicts with a pre-existing mDNS name, a number is automatically appended to the name, e.g.
mymodule-2.local.
Arguments
<name>
- Only valid domain characters are supported: a-z, A-Z, 0-9, -, ..
-
If the # character is the last character in the name, then it is replaced by the last three hex characters of the module's MAC address, e.g. if device MAC address is
4C:55:CC:10:26:05, andmdns.nameisgecko_os-#, then name becomes:gecko_os-605.
Default
gecko_os-#
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Set example
> set mdns.name MyDomain_#
Set OK
Get example
> get md n
MyDomain_#
mdns.service
Abbreviation
md s
Access
get/set
Description
Advertise a module server via mDNS. See Networking and Security, Network Discovery .
The corresponding server must be enabled and configured to auto-start before the service is advertised via mDNS.
Arguments
set syntax
<server name> [<name> [<txt> [<service type>] ] ]
where:
<server name>
|
The name of a Gecko OS server protocol. The following servers are available: |
http
- HTTP server
|
|
tcp
- TCP server
|
|
udp
- UDP server
|
|
remote_terminal
- Remote Terminal server
|
|
<name>
|
An additional name/description of the service. For example:
Sensor HTTP Server
.
To disable advertising of an mDNS service, set the
<name>
argument to
-1
or
disabled
.This also sets the name to
gecko_os#
.
|
<txt>
|
Additional configuration settings for the service. This is a Bonjour style TXT Record, consisting of a string of
set mdns.service http "Test Server" "record1=on.record2=off.another=21"
|
<service type>
|
The service registration type. (Note: .local is appended to the end) By default, the following server/service type is used: |
HTTP server -
_http._tcp.local
|
|
TCP server -
_gecko_os._tcp.local
|
|
UDP server -
_gecko_os._udp.local
|
|
| Remote Terminal server - _telnet._tcp.local |
get syntax
<server name>
where:
<server name>
is one of:
- http
- tcp
- udp
- remote_terminal
- all - list all servers
The response lists the attributes as follows:
"<name>" "<txt>" <type>
e.g.
> get md s http
"Test Server" "record1=on.record2=off.another=21" _http._tcp.local
If
all
is specified to list status of all servers, the response lists the servers and attributes as follows:
<server name> - <name>.type <txt>
...
e.g.
> get md s all
http - Test Server._http._tcp.local record1=on.record2=off.another=21
tcp - my_tcp_server._gecko_os._tcp.local
udp - Disabled
remote_terminal - Disabled
Default
-
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Set example
Advertise tcp service as my_tcp_server
> set md s tcp my_tcp_server
Set OK
> get md s all
http - Disabled
tcp - my_tcp_server._gecko_os._tcp.local
udp - Disabled
remote_terminal - Disabled
Disable advertising of tcp service
> set md s tcp -1
Set OK
> set md s tcp -1
Set OK
> get md s all
http - Disabled
tcp - Disabled
udp - Disabled
remote_terminal - Disabled
Get example
> get md s tcp
"my_tcp_server" "" _gecko_os._tcp.local
mdns.ttl
Abbreviation
md t
Access
get/set
Description
Sets the timeout of the module's mDNS response in seconds: the "Time-to-Live" of a mDNS response from the module. This is essentially a timeout of the validity of a mDNS record. Once expired, a remote client will reprobe the module for an updated response. See Networking and Security, Network Discovery .
Arguments
<seconds>
where
<seconds>
is in the range 1 - 65535.
Default
300
Properties
- network_restart to apply change
Gecko OS Kernel Plugin
Set example
> set mdns.ttl 1000
Get example
> get mdns.ttl
1000