App
app.debug.auto_run
Abbreviation
     
      ap d a
     
    
Access
     
      get/set
     
    
Description
Enable/disable App from auto running.
This variable is not saved. When power is removed the variable is reset to its default value.
By default, an App always runs on power up.
     The
     
      app.debug.auto_run
     
     variable is intended for use only in a debug session, to allow inputting commands to the Gecko OS terminal.
    
Arguments
     
      <1|true|on/0|false|off>
     
    
     where
     
      1
     
     : enable,
     
      0
     
     : disable
    
Default
     
      1
     
    
Properties
- takes effect immediately
 
Supported Platforms
- WGM160P
 
Get example
> get ap d a
1
    Set example
> set app.debug.auto_run 0
Set OK
    app.debug.ignore_settings
Abbreviation
     
      ap d i
     
    
Access
     
      get/set
     
    
Description
This allows manual adjustment of variable settings while debugging a Gecko OS App that loads settings using the API gos_load_app_settings() .
     When
     
      app.debug.ignore_settings
     
     is set, all calls to
     
      gos_load_app_settings()
     
     are ignored. You can then load the Gecko OS app without overwriting test variable settings.
    
Arguments
     
      <1|true|on/0|false|off>
     
    
Default
     
      0
     
    
Properties
- takes effect immediately
 
Supported Platforms
- WGM160P
 
Get example
> get app.debug.ignore_settings
0
    Set example
> set app.debug.ignore_settings 1
Set OK
    app.info
Abbreviation
     
      ap i
     
    
Access
     
      get
     
    
Description
Print information about the current App, including App name, size, SDK version, and running status.
Arguments
     
      -
     
    
Supported Platforms
- WGM160P
 
Get example
> get app.info
SDK version : <SDK version number>
Name        : <App name>
Size        : <Size of app, in bytes>
Running     : <1 = app running, 0 = app not running>