Wireless Serial Port
This application uses two Gecko OS devices each running Gecko OS to demonstrate how to create a wireless serial port. A character typed into the serial port of Module 1 appears instantly at the output of the Module 2 serial port (and vice versa).
Features demonstrated
- Serial Interface Stream Mode
 - Use of the wlan and softap wireless interfaces
 - TCP client and TCP server
 - UDP client and UDP server
 
     
    
Module 1 is configured to start the softap interface and a server on bootup.
Module 2 is configured to use the wlan interface and connect a client to the Module 1 softap server.
The final configuration step places both modules into serial interface stream Mode.
The client/server configuration can use either TCP or UDP protocols.
Wireless Serial Port using TCP
We start by configuring each of the modules, one as a TCP server and one as a TCP client.
Copy and paste the commands in the left hand column of the following table into a Gecko OS terminal connected to Module 1.
Module 1 TCP Server Configuration Settings
| Gecko OS Commands (Module 1) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 1 automatically starts the softap, starts the TCP server, waits for a connection on port 3000 and enters stream mode. Data sent to the Module 1 UART is transmitted over the softap interface.
Now, copy and paste the commands in the left hand column of the following table into a Gecko OS terminal connected to Module 2.
Module 2 TCP Client Configuration Settings
| Gecko OS Commands (Module 2) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 2 automatically connects to the wlan, connects as a client to the TCP server running on Module 1 and enters stream mode. Data sent to the Module 2 UART is transmitted over the wlan interface.
TCP Wireless Magic!
At this point, all characters typed into the Module 1 serial port appear immediately on the Module 2 serial port output (and vice versa). Give it a go, it's like a little piece of wireless magic!
Wireless Serial Port using UDP Client/Server Configuration
The UDP client/server configuration is similar to the TCP configuration, with changes due to the different options available for UDP. We start by configuring each of the modules, one as a UDP server and one as a UDP client.
Copy and paste the commands in the left hand column of the following table into a Gecko OS terminal connected to Module 1.
Module 1 UDP Server Configuration Settings
| Gecko OS Commands (Module 1) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 1 automatically starts the softap, waits for a message on port 8000 and enters stream mode. Data sent to the Module 1 UART is transmitted over the softap interface. However a message from Module 2 is required before Module 1 knows the client address and port.
Now, copy and paste the commands in the left hand column of the following table into a Gecko OS terminal connected to Module 2.
Module 2 UDP Client Configuration Settings
| Gecko OS Commands (Module 2) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 2 automatically connects to the Module 1 softap and enters stream mode. Data sent to the Module 1 UART is transmitted over the wlan interface. On Module 2 sending the first message, Module 1 stores the IP and port of Module 2 for later responses to Module 1.
UDP Wireless Magic!
Type characters into the client (Module 2) Gecko OS terminal. They appear immediately on the Module 1 Gecko OS terminal.
Now type characters into the server (Module 1) Gecko OS terminal. They appear immediately on the Module 2 Gecko OS terminal.
Note : Because UDP is a connectionless protocol, the client must send the first message. Then the server records the address of the client and can respond. If you type first on the Module 1 Gecko OS terminal, there is no response at the Module 2 Gecko OS terminal because the server has no record of a client.
If this is a problem, you can simply set up both modules with a UDP server configuration. See below.
Wireless Serial Port using UDP Symmetrical Server Configuration
UDP is a connectionless protocol, so the terms server and client are used loosely. With Gecko OS, the difference is that a module configured as a UDP server has more options, such as a configurable UDP server port, and some server behavior based on expecting a communication from a client.
If you want either module to be capable of receiving the first communication, just set up both as servers.
Module 1 still runs the softap, but Module 2 has a static IP address and DHCP is not required.
Instead of using a client lock, Module 1 is hard coded with the known IP address and port of Module 2.
Module 1 UDP Server Configuration Settings
| Gecko OS Commands (Module 1) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 1 automatically starts the softap, waits for a UDP message on port 8000 and enters stream mode. Data sent to the Module 1 UART is transmitted over the softap interface to the configured remote host and remote port.
Module 2 UDP Server Configuration Settings
| Gecko OS Commands (Module 2) | Description | 
|---|---|
       
       | 
      
       
       | 
     
On rebooting, Module 2 sets its static IP, joins the WLAN, waits for a UDP message on port 8008 and enters stream mode. Data sent to the Module 2 UART is transmitted over the wlan interface to the configured remote host and remote port.
More UDP Wireless Magic!
Type characters into the Module 1 Gecko OS terminal. They appear immediately on the Module 2 Gecko OS terminal.
Alternatively, type characters into the Module 2 Gecko OS terminal. They appear immediately on the Module 1 Gecko OS terminal.
You can send the first message from either module.
High Speed Connections
The above communications take place with the default UART settings of 115200 baud and no flow control. This is appropriate for a demonstration at human typing speeds. It is possible to use a similar system for high speed communications, for example at UART speeds above 1 Megabaud. In this case it is necessary to configure flow control.
See the High Speed UART app note for examples of configuring baud rates and setting flow control.
Supporting Gecko OS Versions
- Gecko OS 4
 
Change Log
| Modified | Changes | 
|---|---|
| 2019-01-01 | Created |